cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I am using Nucleo F446RE and the acquisition failed with STM32CuneMonitor. Every thing is ok with the prob, processing and variables (Leds green see screen shot) When I launch the Dashboard the start acquiistion button do no thing.

pDABE.1
Associate

The code is a basic blinking LED and a free counter variable. The code runs well on the board. The list of variables is ok in STM32CubeMonitor.Thank you

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
KnarfB
Super User

Strange. Nothing at debug 1? Simplify your flow for debugging, e.g. remove BP bleu node.

hth

KnarfB

pDABE.1
Associate

I already did it without success !! I tried aswell with only on chart and it does'nt works

No message at debug to.

Richard.Chvr
ST Employee

Hello

For sure BP bleu single value node can be removed and ST Chart linked directly to processing node. Can't see the variable you're monitoring in the Monitor-2 screenshot. Can you share a bit more informations about elf and flow?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.