cancel
Showing results for 
Search instead for 
Did you mean: 

Why does the debugger keep disconnecting every 2-5 minutes?

lfish.1633
Associate II

I'm using STM32CubeIDE 1.1.0 with a STEVAL-SPIN3204 board connected via the USB port and onboard ST-Link. About 2-5 minutes after I start a debug session The Console prints "Target is not responding, retrying..." 10 times and then prints "Debugger connection lost.

Shutting down...". At that point I can restart the debugger again sucessfully. Until the debugger starts printing Target is not responding, the debugger works normally. I can single step, run, stop on breakpoints, view and modify variables etc.

This problem occurs even if I merely initiate a debug session and never touch the keyboard so it seems rather unlikely it has anything to do with the program being debugged. And FWIW I did confirm that the watchdog is disabled by the fuse settings.

This discussion is locked. Please start a new topic to ask your question.
13 REPLIES 13

Go into REGEDIT and search for "UpperFilter", you'll usually find a couple of storage related nodes. or "LowerFilter" or "PartMgr"

You're trying to establish the presence of a known problematic driver. Probably not going to want to edit/delete manually unless you're an "IT Guy"

Previously these types of issue with Support Assistant nee PC Doctor

"First I uninstalled 'Dell SupportAssist' and the problem still occurred.

I then uninstalled 'Dell SupportAssistAgent' and the problem went away."

The Intel related troublemaker was "iaStorF" as I recall.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Neither Dell SupportAssist nor SupportAssistAgent is currently installed on my computer. I believe they were deleted by the person who set up all of our computers along with a bunch of other junk that comes preloaded on Dell machines.

I see some UpperFilter keys in HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Control\Class\

value class

USBPcap {36fc9e60-c465-11cf-8056-444553540000}

partmgr {4d36e967-e325-11ce-bfc1-08002be10318}

kbdclass {4d36e96b-e325-11ce-bfc1-08002be10318}

ksthunk {4d36e96c-e325-11ce-bfc1-08002be10318}

mouclass {4d36e96f-e325-11ce-bfc1-08002be10318}

nipbcfk {4d36e97d-e325-11ce-bfc1-08002be10318}

scfilter {50dd5230-ba8a-11d1-bf5d-0000f805f530}

partmgr {53487c23-680f-4585-acc3-1f10d6777e82}

partmgr {53966cb1-4d46-4166-bf23-c522403cd495}

IRENUM {6bdd1fc5-810f-11d0-bec7-08002be2092f}

ksthunk {6bdd1fc6-810f-11d0-bec7-08002be2092f}

volsnaptcvsm {71a27cdd-812a-11d0-bec7-08002be2092f}

ksthunk {ca3e7ab9-b4c3-4ae6-8251-579ef933890f}

spacialGraphFilter d612553d-06b1-49ca-8938-e39ef80eb16f}

wpdUpFltr {eec5ad98-8080-425f-922a-dabf3de3f69a}

value location (inside HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\)

serenum Enum\ACPI\PNP0501\0:

serenum Enum\FTDIBUS\VID_0403+PID_6001+FT3EJVWVA\0000

serenum Enum\FTDIBUS\VID_0403+PID_6001+FT3EJVXNA\0000

serenum Enum\FTDIBUS\VID_0403+PID_6001+FT3EJW3PA\0000

serenum Enum\FTDIBUS\VID_0403+PID_6001+FT3K4221A\0000

serenum Enum\FTDIBUS\VID_0403+PID_6001+FT3K423FA\0000

... several more similar to above, all associated with FTDI usb serial ports

serenum Enum\SNXPCARD_ENUM\SNXPCARD_SERP\1FD4&1999_00011FD4_00E8_Port0

... several more related to

value location (inside \HKEY_LOCAL_MACHINE\SYSTEM\DriverDatabase\DriverPackages\

amdxata amdsata.inf_amd64_ea60132f1a9a7a62\Configurations\amdsata_inst

mshidkmdf capimg.inf_amd64_407f052b0424612c\Configurations\CapImgMini.Inst.NT

mshidkmdf hidi2c.inf_amd64_891a4188cb4bf01b\Configurations\hidi2c_Device.NT

... a few more like that

value location

ibbus ndfltr WinVerbs WinMad mlx4_bus.inf_amd64_cfc8af16c589f850\Configurations\MLX4BUS.DDInstall.NTamd64

... and a bunch more similar keys related to things like that(msports, VWiFibus, pcmcia, etc) that I got tired of listing.

Searching for LowerFilters I found some in HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Control\Class\

related to similar things like EhStorClass, appleLowerFilters, rdyboost, MSRRAS/MINIPORT, Qualcomm, USB serial ports, virtual disk, storflt, etc.

None of this sounds like something that needs to be deleted, why do you think that will help and how do you suggest I determine which ones to delete? Trying one at a time would take hours.

Do you use debug prints over SWO (ITM) ?

-- pa

No.