2022-08-11 6:09 PM
Are there any limitations to how AXI RAM can be partitioned by the linker script?
I have successfully divided SRAM1,2,3 (256K,384K,384K) into two partitions of 512K.
However when I tried:
RAM_EXEC (xrw) : ORIGIN = 0x24000000, LENGTH = 496K
RAM_NOCACHE (xrw) : ORIGIN = 0x2407C000, LENGTH = 528K.DATA_RAM_NOCACHE :
{ . = ALIGN(4);
_snocachedata = .;
*(.DATA_RAM_NOCACHE)
*(.DATA_RAM_NOCACHE*)
. = ALIGN(4);
_enocachedata = .;
} >RAM_NOCACHE
_sinocachedata = LOADADDR(.DATA_RAM_NOCACHE);and in the startup
...
/* stack used for SystemInit_ExtMemCtl; always internal RAM used */
.word _sinocachedata
/* start address for the .data section. defined in linker script */
.word _snocachedata
/* end address for the .data section. defined in linker script */
.word _enocachedata
...
ldr r0, =_snocachedata
ldr r1, =_enocachedata
ldr r2, =_sinocachedata
movs r3, #0
b LoopCopyDataInit
...The Build analyser in cubeIDE reports back the expected areas after compilaiton but when executing code a MEM Handler Exception is thrown...
2022-08-11 8:02 PM
Debug and step the code?
Generate a disassembly / listing file walk the codes/values ?