cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link Not Detected in CubeIDE 1.13.1 on MacOS

EliKrumholz
Associate

Hello, after upgrading from 1.12.1 to 1.13.1 I am unable to debug a project with a Nucleo-G431 development board. Downgrading back to 1.12.1 works as a temporary workaround.

The issue appears to be isolated to STM32CubeIDE, I am still able to detect and connect to the ST-Link to upgrade the ST-Link firmware (oddly, the upgrade tool inside STM32CubeIDE 1.13.1 works), and STM32CubeProgrammer also can connect with no issues.

I am using an M2 Macbook Air running MacOS 13.5.1. I previously tried reinstalling STM32CubeIDE 1.13.1 (including the ST-Link server software), but that did not fix the issue.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0