cancel
Showing results for 
Search instead for 
Did you mean: 

Login issue within the IDE

JB_Dev
Associate II

Hey all, first and foremost I'm new to the embedded systems space, I've been trying to get my feet wet with a hello world project but for some reason with Cube 1.17.0 I'm missing the "MyST" login tab at the top of the screen. I've tried Re-installing thinking I had done something wrong during the original process to no avail. For further context I have a Linux system with the IDE installed and code generation worked properly on it however I found endless issues with the debugger and decided it might be an issue with Linux so I gave up and installed it into my windows machine to see if that helped with anything and now this is my new issue. To get around this issue as the ide suggested I navigated to "Help->stm32Cube Updates->Connection to my ST" and logged in through there and tried to create a new project and still it gave me the error as if I wasn't signed in, tried the same method again and it told me my session had expired, I haven't tried code generation just yet because as far as I understand I need to be logged in to do so I imagined it would be a wasted effort but I will report back after an attempt to do so. I'm not sure if the Linux install is a previous version as well but it may be the case

 

Any help would be appreciated Thanks!

11 REPLIES 11

Hey all! I know I'm a little late to the party but I found a quick fix for anyone in a bind - if you login and speed run making a project it will generate the code before you are signed out!

phil2nice
Associate II

I am new too with stm32 devs.

i followed everything, installation, create new stm32 project: ....  right away it failed 

You ST dev team ...... you should try or test your software !!!!!!