2025-06-11 11:54 PM
I am having trouble running a virtual machine on STM32H747I-DISCO. I followed the example on GitHub (https://github.com/CPDev-ControlProgramDeveloper/VirtualMachine/tree/main/Platforms/STM32/CubeIDE_F446). I feel like my program is almost 1:1, but when I try to run it, it doesn't work. Here is "my" code:(https://github.com/domic1/include_CPDev1).
The program's operation is very random; sometimes it stops at the timer, and sometimes at loading the program. I wonder if the problem is in the code or in the debugger.