2026-01-16 4:04 AM - last edited on 2026-01-16 4:23 AM by Andrew Neil
Hello, I need a clear step by step guide on how to set up Pnucleo lrwan 3 end node and gateway and connect both to the loriot server. currently I have issues communicating with my END node using the AT command via terminal.
My other issue is that; the PNUCLEO lrwan 3 antenna is 480MHz, but when I check the paramaters of the device using terminal, I discover that the frequency is EU-868MHz, so now I have to reconfigure the device tp the right frequency, how do I do this. I have consulted the UM2587 material but it does not appear to be so clear to me.
2026-01-16 4:58 AM
Note that the P-NUCLEO-LRWAN3 is Not Recommended for New Designs (NRND), and has been for a long time now:
And the Gateway was never suitable for deployment.
See: