2021-02-10 5:38 AM
void write_max (uint8_t address, uint8_t data)
{
HAL_GPIO_WritePin (cs_GPIO_Port, cs_Pin, GPIO_PIN_RESET); // pull the CS pin LOW
write_byte (address);
write_byte (data);
HAL_GPIO_WritePin (cs_GPIO_Port, cs_Pin, GPIO_PIN_SET); // pull the CS pin HIGH
}
void display_value(uint8_t address, uint32_t number, uint8_t dp_at){
uint8_t k = 0;
dp_at++;
if (number > 0) {
for (int x = address; number != 0; ++x) {
k = number % 10;
k = dp_at==x ?(k|0b10000000):k;
write_max(x,k);
number = number/10;
}
} else {
number = dp_at>1 ? number|0b10000000 : number;
write_max(address,number);
}
}
void display_floatvalue(float Value,uint8_t precision){
uint32_t prmultiplayer=0,partInt=0,fractional=0;
uint8_t ndigit = 1,k=0;
prmultiplayer = pow(10,precision);
partInt = floorf(Value);
fractional = (Value-partInt)*prmultiplayer;
if(fractional>0){
while(fractional != 0){
k = fractional % 10;
write_max(ndigit,k);
fractional = fractional/10;
ndigit++;
}
}else {
write_max(1,0);
}
k = ndigit-1;
display_value(ndigit,partInt,k);
}
int main(void){
while(0){
led_desplay_float(0.001);
}
}above code not work properly
led_desplay_float(0.001);
but it shows 0.1
so how can i display exact value 0.001
2021-02-10 11:50 AM
use sprintf?
2021-02-10 8:50 PM
I have tried this function but not work.
above code works fine ex 12.345 , 2 it shows 12.34
if i input ex 0.01 , 2 it shows 0.1 wrong value not add zero before 1.
2021-02-10 9:00 PM
sprintf and friends should work with float if you supply "-u _printf_float" as a linker option. There is a check box in the STM32CubeIDE C Build Tool Settings.
2021-02-10 10:43 PM
Apart from the need to have a libc version with floating point print support ...
You are using a wild mixture of float and double all around in your code and your posts.
Are you aware of the differences ?
sprintf (buf,"%8.3f", (double) fvar);
POSIX supports only double arguments for the e,E,f,F,g,G conversions. The Cube-supported lib might be different.