Skip to main content
a.niggebaum
Visitor II
August 5, 2019
Question

CubeMX Plugin does not maintain custom include paths upon re-generation of code in CubeIDE projects

  • August 5, 2019
  • 6 replies
  • 1991 views

Since my upgrade to CubeIDE version 1.0.2 (build 3566_20190716-0927, cubeMX version 5.3.0.201908220903), my own include paths for the MCU GCC compiler are deleted/not kept when the CubeMX plugin re-generates code. I can isolate the behavior:

  1. Create new STM32 project with any MCU
  2. In the project properties go to "C/C++ Build/Settings/Tool Settings/MCU GCC Compiler/Include paths" and add a custom path to the list. Apply and Close
  3. Open the .ioc file with the CubeMX perspective and change any pin configuration. Save and re-generate code
  4. The previously added path is no longer available in the list.

Does anyone have the same issue and can re-create this behavior?

Thank you very much for your help.

This topic has been closed for replies.

6 replies

JVan.17
Visitor II
August 5, 2019

Here too

ldecicco
Visitor II
August 5, 2019

I can confirm this really annoying bug is also affecting my installation of STM32CubeIde 1.0.2 on linux.

Associate
August 5, 2019

I confirm too.

It seems that when CubeIDE regenerates the code, it eliminates and entirely replaces all the Build Configurations with two new Debug and Release; really annoying!

JVan.17
Visitor II
August 9, 2019

Also my preprocessor symbols are missing

RLeon.230
Visitor II
October 19, 2019

I have the same problem.

My workaround:

- Start from a working version of the project.

- Doubleclick .ioc

- Change perspective

- Migrate

- Project -> Properties -> C/C++ General -> Paths and Symbols -> Includes -> Export Settings // Say includes_1.txt

- Project -> Properties -> C/C++ General -> Paths and Symbols -> Source Location -> Print screen and save in Paint

- Project -> Generate Code

- Project -> Properties -> C/C++ General -> Paths and Symbols -> Includes -> Export Settings // Say includes_2.txt

- Merge includes_1.txt and includes_2.txt // Say includes_3.txt

- Project -> Properties -> C/C++ General -> Paths and Symbols -> Includes -> Import Settings // Select includes_3.txt

- Project -> Properties -> C/C++ General -> Paths and Symbols -> Source Location -> Merge according the picture saved in Paint

- Build and run

Associate II
January 31, 2025

I'm also having this issue, in my scenario i create a project in STM32CubeMX_6.13.0 and generate the project after this i added a paths in paths and symbols and again i edit the IOC in STM32CubeMX and try to Re-generate the project but it shows ERROR POPUP  like thisERROR POPUPERROR POPUP

 after this i try build but it didn't build errors are came like this total 40 error all are Hal and oskernal error
   D:/NAVANEETHAN/CoffeeMaker/DisplayControl/Project/DisplayControl/CM7/Core/Src/main.c:116: undefined reference to `HAL_Init'

any one help me for this issue
Thank you