cancel
Showing results for 
Search instead for 
Did you mean: 

CODE DUMPING ISSUE

sram.1
Associate II

 

STMicroelectronics ST-LINK GDB server. Version 7.3.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.

Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled

Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Encountered Error when opening D:\stmd\STM32CubeIDE_1.12.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.600.202301161003\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Shutting down...
Exit. 

 

I tried uninstalling and reinstalling 2-3 times and i changed the path. but i am getting the same error. Please give me a solution.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Souhaib MAZHOUD
ST Employee

Hi @sram.1 

Thank you for posting!

I advise to try using the last version of STM32CubeIDE 1.13.1, otherwise could you share the name of the board you using.

Thank you

Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.