cancel
Showing results for 
Search instead for 
Did you mean: 

Build Analyzer issue

matt-crc
Senior III

Hello,

Is there a trick to get the Build Analyzer to produce data every time the code is compiled?   It seems like the only way I can get it to update the window is if I change something in the linker script file and recompile again.   Is there an easier way or a setting that needs to be set?

thanks

Matthew

 

21 REPLIES 21

I can confirm. It seems the trick is to:

  • Right click on project name and Select Refresh
limited_processing
Associate

This is an incredibly frustrating bug. 

For me, none of the clicking and refreshing of the project works. The only alternative to rebooting the entire IDE I've found is to close the build analyzer before building, then building, then re-opening it from the Window menu and refreshing.