cancel
Showing results for 
Search instead for 
Did you mean: 

Adding an SPI port to an existing ST project

TCris.1
Associate II

Hi All,

I am new to the IDE Cube and I would like to know what is the most appropriate method to add an SPI to an existing Cube project ?

I am specially interested in the people counter firmware running on the Nano boards, to witch I am not able to add an SPI.

The device configuration tool does not open with the code provided by ST .

Adding the files manually, runs into a lot of problems.

Thank you in advance,

Cristian

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
KnarfB
Super User

Do you mean STSW-IMG010 software? Whcih comes with an NucleoF401RE_53L1_Expansion.ioc file? What exactly did you try and want to achieve?

TCris.1
Associate II

Yes, it is about STSW-IMG010 .

I need to send over the SPI1 the counting number. I just need to initialize the SPI1 but I'm not able yet to make it work.

I am new to Cube IDE and it seems that I am missing something....

Cristian

TCris.1
Associate II

I get the ERROR:

C:/Users/RFLab/STM32CubeIDE/workspace_1.4.0/en.STSW-IMG010/Src/main.c:250: undefined reference to `HAL_SPI_Transmit'

I read on the web that it could be related to a "c" file that is missing or not in the correct path....

Please see attached the code:

Thank you,

Cristian