2025-09-08 11:29 AM
Hello,
I am trying to get SWO output working in VSCode using the Cortex-Debug plugin (v1.12.1).
My setup:
Debugger: STLink V3-MINIE
MCU: STM32H747IIT6
IDE: VSCode with Cortex-Debug
GDB Server: OpenOCD
Debug config: Trace Asynchronous SW enabled in CubeMX
When I run the project in STM32CubeIDE, the SWO output works as expected.
However, in VSCode I don’t see any SWO output in the terminal.
I overrode the write function like this:
int _write(int file, char *ptr, int len) {
int dataIdx;
for (dataIdx = 0; dataIdx < len; dataIdx++) {
ITM_SendChar(*ptr++);
}
return len;
}My launch.json:
{
"name": "CM7 SWO",
"cwd": "${workspaceRoot}/CM7",
"type": "cortex-debug",
"executable": "build/Printf_CM7.elf",
"request": "launch",
"servertype": "openocd",
"gdbPath": "/opt/ST/STM32CubeCLT_1.19.0/GNU-tools-for-STM32/bin/arm-none-eabi-gdb",
"device": "STM32H747IITx",
"svdFile": "/opt/ST/STM32CubeCLT_1.19.0/STMicroelectronics_CMSIS_SVD/STM32H747_CM7.svd",
"configFiles": [
"interface/stlink.cfg",
"target/stm32h7x.cfg"
],
"runToEntryPoint": "main",
"preLaunchTask": "Build All Debug",
"showDevDebugOutput": "raw",
"swoConfig": {
"enabled": true,
"source": "socket",
"swoFrequency": 2000000,
"cpuFrequency": 480000000,
"decoders": [
{
"port": 0,
"type": "console"
}
]
}
}When I launch debugging, I get this error message from the GDB server:
marus25.cortex-debug-1.12.1/support/openocd-helpers.tcl:
Error: Could not find TPIU/SWO names. Perhaps it hasn't been created?Does anyone know what I might be missing in the launch.json or OpenOCD configuration to get SWO working with Cortex-Debug and STLink V3-MINIE?
Thanks in advance!
Best regards
OskarP.
Solved! Go to Solution.
2025-10-03 3:44 AM
2025-10-06 12:12 AM
@Cartu38 OpenDev and @Nawres GHARBI Thank you very much for your help. I will wait until SWO support is added and use liveWatch until then, as I really like the new extension.
Best regards
Oskar