2025-05-13 8:33 PM - edited 2025-05-13 9:00 PM
Hi,
I want to add some functions to the FP-AI-MONITOR1 project, but I prefer to compile it using CMake for better compatibility with AI agents and the STM32Cube VS Code extension.
I’ve created the CMakeLists.txt files and successfully compiled the project. However, the firmware doesn’t run as expected compared to when I compile it using STM32CubeIDE.
It gets stuck after calling HAL_Delay(1000); if any of the following code blocks are not commented out:
if (SysDebugInit() != 0) {
sys_error_handler();
}if (xTaskCreate(InitTaskRun, "INIT", INIT_TASK_CFG_STACK_SIZE, NULL, INIT_TASK_CFG_PRIORITY, &s_xTheSystem.m_xInitTask) != pdPASS) {
xRes = SYS_OUT_OF_MEMORY_ERROR_CODE;
SYS_SET_SERVICE_LEVEL_ERROR_CODE(xRes);
}Both lines of code are in SysInit function in sysinit.c file.
Can anyone tell me what might be causing this error? Also, is there an easy way to convert an STM32CubeIDE project into a CMake project or into STM32CubeMX ioc file? I need to use Manus AI to generate the CMakeLists.txt files that include all the necessary files for compilation. Thank you.
2025-05-14 3:23 AM
Hi @deddy11
I'm currently traying to export this project to VSCode and check if I have the same issue but at first sight I think you have an issue with the file initializing your systick maybe an msp setting the timer as systick source
2025-05-14 9:45 PM
Hi @Nawres GHARBI
Thanks for you response. I have tried to use SystemClock_Config functions both from FP-AI-Monitor1 and from other project, but both get stuck. I'll wait for your result. Thanks.
2025-05-15 1:23 AM
could you please share your systick, timing and interrupts config please ?
2025-05-15 1:41 AM - edited 2025-05-15 1:53 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.