Question
STM32MP157 in KEIL error.
Hello.
I use a board STM32MP157A-DK1. I have SD-card with linux and now i try to run the board in KEIL. I have read file "Using STM32MP1 Cortex-M with Keil MDK". But I get error:
Error: flash download failed.
Also a can see:
Full ship erase done.
No Algorithm found for: 0000000H - 000003BBH
No Algorithm found for: 1000000H - 1000147FH
Programming skiped.
I think that (if i enter options - utilites - settings - add) I have to add the correct algorithm but I get the algorithm whatever i choose. Maybe may I download the correct algorithm?