2021-10-19 3:31 AM
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157DAB Re v.Z,
SN : 004700213438511336383238
FW version : 0x0110
Device ID : 0x0500
Start operation done successfully at partition 0x03
Error:
Error: unable to get the associate alternate setting of partition ID: 0xf1
Error: please make sure that your alternate settings have string descriptors with the right format
Error: unable to upload data from virtual partition
Received PhaseID == 0xFF, system is going to reboot
CubeProgrammer version is 2.7.0
TSV file is:
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 tf-a-stm32mp157a-stm32mp151-dk1-mx-usb.stm32
- 0x03 fip-boot Binary none 0x0 fip-stm32mp157a-stm32mp151-dk1-mx-trusted.bin
P 0x04 fsbl1 Binary mmc0 boot1 tf-a-stm32mp157a-stm32mp151-dk1-mx-emmc.stm32
P 0x05 fsbl2 Binary mmc0 boot2 tf-a-stm32mp157a-stm32mp151-dk1-mx-emmc.stm32
P 0x06 fip Binary mmc0 0x00080000 fip-stm32mp157a-stm32mp151-dk1-mx-trusted.bin
PE 0x10 env Binary mmc0 0x00480000 none
P 0x11 bootfs System mmc0 0x00500000 st-image-bootfs-openstlinux-weston-stm32mp1-duck.ext4
P 0x12 vendorfs FileSystem mmc0 0x04500000 st-image-vendorfs-openstlinux-weston-stm32mp1-duck.ext4
P 0x13 rootfs FileSystem mmc0 0x05500000 st-image-weston-openstlinux-weston-stm32mp1-duck.ext4
P 0x14 userfs FileSystem mmc0 0x33F00000 st-image-userfs-openstlinux-weston-stm32mp1-duck.ext4
There ar no any problems downloading this file in Windows7 with same CubeProgrammer version.
Could you please give an Idea what may be wrong?
Thank you in advance
Looking forward for your reply
Solved! Go to Solution.
2022-08-29 6:32 AM
Yes. Problesm was solved. In my case it was VmWare virtual machine running on the same PC, that take control over USB each time target board restartes. After stopping VM problem was disappeared.
2021-10-26 2:38 AM
Hi @ASkri.1 ,
Sorry for late reply ..
Are you still fighting with this issue or find a way to fix/workaround it ?
Olivier
2021-10-26 3:33 AM
2021-10-26 6:42 AM
Hi @ASkri.1 ,
Ok so I understand you already refer to troubleshooting guide on wiki such as https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer#How_to_proceed_when_the_DFU_driver_installation_fails_on_Windows_host_PC
https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer#How_to_check_if_the_DFU_driver_is_functional
Searching for other case presenting the same error message I found 2 occurence :
-> looks dependent on the presence of STLink cable ?
What about your case ?
Else, internally we sometime faced similar issue the first time we program an SDCard with FIP partition ( DV3.0) while SDCard was previously partionned and programed with legacy ( TF-a, Uboot)
Let me know if you are in one of that case
Olivier
2021-11-11 1:15 AM
Hi, Olivier!
So, there are following update:
Trying to download flashlayout file. Waiting to stuck on error after programming partition 0x02:
RUNNING Program ...
PartID: :0x03
Reconnecting the device ...
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157DAB Rev.Z,
SN : 003F00313438511336383238
FW version : 0x0110
Device ID : 0x0500
Start operation done successfully at partition 0x03
Error: an error occured while uploading data from the virtual partition 0xF1
Received PhaseID == 0xFF, system is going to reboot
Then, disconnect USB cable and connect it back (without powering down target board), start again.
STM32CubeProgrammer continue to download partitions 0x04 , 0x05, 0x06 (tf-a, fip1, fip2) and then stuck again on partitoon 0x10:
Error: failed to download Segment[0]
Error: failed to download the File
Error: Download partition 0x10 failed
Error: TSV flashing service failed
And error from U_BOOT side:
UPLOAD ... done
Ctrl+C to exit ...
########DOWNLOAD ... OK
Ctrl+C to exit ...
#
UPLOAD ... done
Ctrl+C to exit ...
#
UPLOAD ... done
Ctrl+C to exit ...
dfu_write: Wrong sequence number! [1] [0]
And next restart of STM32CubeProgrammer completes process with last 0x10 partition (UBI image)
Now board can be booted from SPI flash.
Have tried to download image to eMMC - with such trick - also ok. So, seems, that there is DFU reconnect
error before or after loading partition 0x03.
Could you please help me to avoid it.
I want to point again, that there are no such (any) problems with Windows 7 (Core i5/i7 MCU both tested).
Thank you in advance.
Looking forwared for your reply.
2022-08-29 6:29 AM
same issue on my custom board. do someone have any progress with that?
2022-08-29 6:32 AM
Yes. Problesm was solved. In my case it was VmWare virtual machine running on the same PC, that take control over USB each time target board restartes. After stopping VM problem was disappeared.
2022-08-29 7:28 AM
I don't run VM . and with old dunfell flashlayout it working fine. very strange behavior . tnx btw
2024-05-17 3:11 AM
I am on Windows and VMWare too, but even with virtual machined off , the issue persists (STMProgrammer v.2.16.0)