Issue to program MMC using STM32_Programmer_CLI tool
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-16 1:44 AM
Hello,
I am facing an issue with flashing my MMC on STM32MP157C-DK2 board using STM32_Programmer_CLI (linux version)
I have created a flash layout file like this:
#opt Id Name Type Device Offset Binary
- 0x01 fsbl-boot Binary none 0x0 tf-a-loader.stm32
- 0x03 ssbl-boot Binary none 0x0 u-boot-loader-optee.stm32
P 0x04 fsbl1 Binary mmc0 0x4400 tf-a.stm32
P 0x05 fsbl2 Binary mmc0 0x00044400 tf-a.stm32
P 0x06 ssbl Binary mmc0 0x00084400 u-boot.stm32
P 0x07 teeh Binary mmc0 0x00184400 tee-header_v2.stm32
P 0x08 teed Binary mmc0 0x001C4400 tee-pageable_v2.stm32
P 0x09 teex Binary mmc0 0x00204400 tee-pager_v2.stm32
P 0x10 ssbl-env Binary mmc0 0x00244400 u-boot-env.bin
P 0x11 ssbl-env-red Binary mmc0 0x00246400 u-boot-env.bin
P 0x12 fit1 Binary mmc0 0x00248400 fit_kernel_dtb.itb
P 0x13 rfs1 Binary mmc0 0x00848400 rootfs.squashfs
P 0x14 fit2 Binary mmc0 0x02048400 fit_kernel_dtb.itb
P 0x15 rfs2 Binary mmc0 0x02648400 rootfs.squashfs
After loading tf-a and u-boot and starting U-Boot in RAM, U-Boot fails to load binaries for flashing them into MMC
If I use a tsv file (with RawImage of SDcard as defined bellow), there is no issue but I don't want to choose this option because of time issue. Downloading and burning a complete image of MMC takes more time than downloading and burning individually images.
Partitions size is bigger than images size.
#opt Id Name Type Device Offset Binary
- 0x01 fsbl-boot Binary none 0x0 tf-a-loader.stm32
- 0x03 ssbl-boot Binary none 0x0 u-boot-loader-optee.stm32
P 0x32 sdcard RawImage mmc0 0x0 sdcard.img
Here are the logs of STM32_Programmer_CLI:
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 0035002E3338510B39303435
FW version : 0x0110
Device ID : 0x0500
Device name : STM32MPxxx
Device type : MPU
Device CPU : Cortex-A7
Start Embedded Flashing service
Memory Programming ...
Opening and parsing file: tf-a-loader.stm32
File : tf-a-loader.stm32
Size : 245384 Bytes
Partition ID : 0x01
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:03.103
RUNNING Program ...
PartID: :0x01
Start operation done successfully at partition 0x01
Flashlayout Programming ...
[==================================================] 100%
Running Flashlayout Partition ...
Flashlayout partition started successfully
Memory Programming ...
Opening and parsing file: u-boot-loader-optee.stm32
File : u-boot-loader-optee.stm32
Size : 810605 Bytes
Partition ID : 0x03
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:08.610
RUNNING Program ...
PartID: :0x03
reconnecting the device ...
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x0000
SN : 0035002E3338510B39303435
FW version : 0x0110
Device ID : 0x0500
Start operation done successfully at partition 0x03
Error: an error occured while uploading data from the virtual partition 0xF1
Received PhaseID == 0xFF, system is going to reboot
Here are the U-Boot Logs:
U-Boot 2018.11-stm32mp-r4 (Nov 14 2018 - 16:10:06 +0000)
CPU: STM32MP157CAC Rev.B
Model: STMicroelectronics STM32MP157C-DK2 Discovery Board
Board: stm32mp1 in op-tee mode (st,stm32mp157c-dk2)
Board: MB1272 Var2 Rev.C-01
DRAM: 480 MiB
Clocks:
- MPU : 650 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
****************************************************
* WARNING 500mA power supply detected *
* Current too low, use a 3A power supply! *
****************************************************
NAND: 0 MiB
MMC: STM32 SDMMC2: 0, STM32 SDMMC2: 1
In: serial
Out: serial
Err: serial
Net: eth0: ethernet@5800a000
Hit any key to stop autoboot: 0
Boot over usb0!
partitions : Writing GPT: success!
done
DFU alt info setting: done
crq->brequest:0x0
crq->brequest:0x0
I don't have any information in LOGs helping me to understand what is the problem.
Does anyone know what is wrong in the first tsv file ?
Best regards,
Sebastien
- Labels:
-
STM32CubeProgrammer
-
STM32MP15 Lines
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-04-22 6:27 AM
Hi @sbg29
As a first hint could you please manage to get a proper supply voltage.
Seems you are using a weak one
****************************************************
* WARNING 500mA power supply detected *
* Current too low, use a 3A power supply! *
****************************************************
We already have cases where this lead to erratic behavior during flash operation.
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.