2019-10-20 2:16 PM
Hello,
I am running example "OpenAMP_TTY_echo" on the board "stm32mp157c-dk2"
I have modified the code a little bit so that channel0 (uart0) doesn't have to wait for a massage from linux side and transmit message every half second. It is sending the messages on every half second without problem.But the problem is now uart1 is not working. I mean on linux side if I write "echo "Hello Virtual UART1" >/dev/ttyRPMSG1" , I can not receive any callback message from the console. This means channel 1 is not working because channel 0 is blocking it. Is it normal ? Why normal ?
while (1)
{
OPENAMP_check_for_message();
" "
" "
VIRT_UART_Transmit(&huart0, Data, size);
HAL_Delay(500);
if (VirtUart1RxMsg) {
VirtUart1RxMsg = RESET;
VIRT_UART_Transmit(&huart1, VirtUart1ChannelBuffRx, VirtUart1ChannelRxSize);
}
}
Solved! Go to Solution.
2019-10-25 1:20 AM
Hello,
I managed to reproduce and i found an issue in the MAILBOX_Poll function in OpenAPM_TTY_echo/Src/mbox_ipcc.c.
This function treats either a buffer free or a new message event but not both. As a buffer free event is received each time a rpmsg is sent from Cortex-M4, the message received event is never considered and the variable is never set. It will be fixed in a future version but if you want to fix it in your code you can replace the MAILBOX_Poll function by this one :
/**
* @brief Initialize MAILBOX with IPCC peripheral
* @param virtio device
* @retval : Operation result
*/
int MAILBOX_Poll(struct virtio_device *vdev)
{
/* If we got an interrupt, ask for the corresponding virtqueue processing */
int ret = -1;
if (msg_received_ch1 == RX_BUF_FREE) {
OPENAMP_log_dbg("Running virt0 (ch_1 buf free)\r\n");
rproc_virtio_notified(vdev, VRING0_ID);
msg_received_ch1 = RX_NO_MSG;
ret = 0;
}
if (msg_received_ch2 == RX_NEW_MSG) {
OPENAMP_log_dbg("Running virt1 (ch_2 new msg)\r\n");
rproc_virtio_notified(vdev, VRING1_ID);
msg_received_ch2 = RX_NO_MSG;
/* The OpenAMP framework does not notify for free buf: do it here */
rproc_virtio_notified(NULL, VRING1_ID);
ret = 0;
}
return ret;
}
BR,
Calvin
2019-10-25 1:20 AM
Hello,
I managed to reproduce and i found an issue in the MAILBOX_Poll function in OpenAPM_TTY_echo/Src/mbox_ipcc.c.
This function treats either a buffer free or a new message event but not both. As a buffer free event is received each time a rpmsg is sent from Cortex-M4, the message received event is never considered and the variable is never set. It will be fixed in a future version but if you want to fix it in your code you can replace the MAILBOX_Poll function by this one :
/**
* @brief Initialize MAILBOX with IPCC peripheral
* @param virtio device
* @retval : Operation result
*/
int MAILBOX_Poll(struct virtio_device *vdev)
{
/* If we got an interrupt, ask for the corresponding virtqueue processing */
int ret = -1;
if (msg_received_ch1 == RX_BUF_FREE) {
OPENAMP_log_dbg("Running virt0 (ch_1 buf free)\r\n");
rproc_virtio_notified(vdev, VRING0_ID);
msg_received_ch1 = RX_NO_MSG;
ret = 0;
}
if (msg_received_ch2 == RX_NEW_MSG) {
OPENAMP_log_dbg("Running virt1 (ch_2 new msg)\r\n");
rproc_virtio_notified(vdev, VRING1_ID);
msg_received_ch2 = RX_NO_MSG;
/* The OpenAMP framework does not notify for free buf: do it here */
rproc_virtio_notified(NULL, VRING1_ID);
ret = 0;
}
return ret;
}
BR,
Calvin
2019-10-25 5:06 AM
Thank you very much