cancel
Showing results for 
Search instead for 
Did you mean: 

When issuing the shutdown command the BUCK3 VDD regulator used for IO is not turned off.

SKris
Associate III

When we tried the shutdown command ( shutdown -hP now ) from the debug console, all the PMIC regulators are turned off, except for the BUCK3 VDD regulator used for IO.

Both our custom board which uses STPMIC1E and the STM32MP157F-eval board which has STPMIC1A have the same behavior.

Is there any configuration which is not letting it to be turned off?

Any help is much appreciated.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Kevin HUBER
ST Employee

Hello @SKris​ ,

It looks like your board is just going into standby mode. Please can you follow the best answer from this community post: https://community.st.com/s/question/0D53W00001JAWO4SAP/steps-to-lowest-power

You have to modify the DTS to allow a real system shutdown.

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Kevin HUBER
ST Employee

Hello @SKris​ ,

It looks like your board is just going into standby mode. Please can you follow the best answer from this community post: https://community.st.com/s/question/0D53W00001JAWO4SAP/steps-to-lowest-power

You have to modify the DTS to allow a real system shutdown.

Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
SKris
Associate III

Hi Kevin,

Thanks a lot for sharing the link.

The suggested changes to the tf-a device tree worked for us, now we see the buck3 being turned off when shutdown command is executed.

Thanks,

Shalini