cancel
Showing results for 
Search instead for 
Did you mean: 

Error during repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15

SFuch.1
Associate III

Hello,

I try to install the distribution package using

repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15

as described in the wiki, before that made sure to install all packages mentioned in the prerequisites page.

The command fails with:

File "/home/steffen/Kirkstone/Distribution-Package/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/.repo/repo/main.py", line 79

   file=sys.stderr)

       ^

SyntaxError: invalid syntax

I am using Ubuntu 20.1, my python version is 3.8.10

Does anyone know what I am missing?

Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Kevin HUBER
ST Employee

Hello @SFuch.1​ ,

I tried on my side and the command seems to work and I also use python 3.8.10.

Did you try to remove the .repo file and remake " repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15 " ?

Maybe there was a problem during this part.

Best Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NEW ! Sidekick STM32 AI agent, see here