cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157F: stm32-mdma.c fast (overlapped) DMA transaction problem (Linux)

GLaure
Senior

Hi!

We are using mdma (dma0chan20) to do "memory to memory" transfers from the FMC to (user) RAM. The FMC is used to access a FIFO buffer that is filled by an FPGA (128kB size).

Between individual DMA transactions we measure a delay up to 5ms leading to a buffer overrun in the FIFO.

I tried to improve this by scheduling a second DMA transfer directly after the first. I assumed that this "overlapped" transfer will automatically start when the first completes and therefore reduce the time between DMA transfers.

This did not work as I assumed:

I get the dma_completed callback of the first transaction, but the second (overlapped) transfer does not seem to get started.

Info: I put a dev_dbg into stm32_mdma_irq_handler and it is never called by the overlapped transaction. Only by the first one.

Funny fact:

When I change the used dma_channel to "dma2chan0" and using the "dma" (and not "mdma" engine) it works. The overlapped transfers work and all dma_completed get called.

So far so good, but:

The transfer speed of "dma2chan0" seems to be a lot slower. Overlapping works but the FIFO overruns anyway, because a running dma transaction is not able to transfer the data in time.

I looked into stm32-mdma.c and did not see any code prohibiting my use case. But in the MPU reference manual I read this:

MDMA_CxCR Bit 0 "EN" Channel enable:

When this bit is read as 0, the software is allowed to program the configuration registers. It

is forbidden to write these registers when the EN bit is read as 1 (writes are ignored).

Is this the root my problem?

Update: I just checked: CCR Bit 0 is "1" on overlapped transfers.

Is there another way to reduce the DMA setup time between individual DMA transactions?

I thought about using a second dma_channel (dma0chan21) for overlapping transactions. So prepare it, hold it back until the other channel (dma0chan20) calls dma_completed. And then the other way around.

Bye Gunther

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0