cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP1 FIP generation with the TF-A compilation failure

NRixh.1
Associate

Hello ST community,

For a project, we use the STM32MP157F-EV1 where we are trying to implement the secure boot chain. For this, we have to generate a FIP package that contains all required certificates.

In the ST wiki two methods are proposed :

  1. One using the FipTools and cert_create
  2. Using the TF-A make system to generate the FIP.

The second method doesn't work from my side. I have a build error. Here is my modus operandi :

  • Source the STM32MP1 toolchain
./opt/st/stm32mp1/3.1-openstlinux-5.10-dunfell-mp1-21-03-31/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi
  • Go to the TF-A source directory
cd <Developer_Package_directory>/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-2.4.r1-r0/tf-a-stm32mp-2.4.r1
  • Launch the build of TF-A as specified in the wiki :
make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1  \       MBEDTLS_DIR=~/mbedtls  \
AARCH32_SP=sp_min  \
BL33=../../u-boot-stm32mp-2020.10.r1-r0/deploy/u-boot-nodtb-stm32mp15.bin BL33_CFG=../../u-boot-stm32mp-2020.10.r1-r0/deploy/u-boot-stm32mp157f-ev1-trusted.dtb  \
DTB_FILE_NAME=stm32mp157f-ev1.dtb         TRUSTED_BOARD_BOOT=1 GENERATE_COT=1 ROT_KEY=<private_key_path>
  • The build output is :
Including bl32/sp_min/sp_min.mk  LD   /home/ag/STM32mp1_Ecosystem_5.10/Developer_Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-2.4.r1-r0/tf-a-stm32mp-2.4.r1/build/stm32mp1/release/bl32/bl32.elfarm-ostl-linux-gnueabi-ld.bfd: 
unrecognized option '-Wl,-O1'arm-ostl-linux-gnueabi-ld.bfd: use the --help option for usage informationmake: 
*** [Makefile:1122: /home/ag/STM32mp1_Ecosystem_5.10/Developer_Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/tf-a-stm32mp-2.4.r1-r0/tf-a-stm32mp-2.4.r1/build/stm32mp1/release/bl32/bl32.elf] Error 1

This output makes me think that LDFLAGS that shall be given to GCC are given to LD directly. Does anyone have an idea of why this procedure doesn't work?

Many thanks for considering my request.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
OlivierK
ST Employee

Hi NRixh.1 (Community Member) 

Yes indeed, as described here:

https://wiki.st.com/stm32mpu/wiki/How_to_configure_TF-A_BL2

unset LDFLAGS;

unset CFLAGS;

then lauch the build.

Regards,

Olivier

View solution in original post

2 REPLIES 2
OlivierK
ST Employee

Hi NRixh.1 (Community Member) 

Yes indeed, as described here:

https://wiki.st.com/stm32mpu/wiki/How_to_configure_TF-A_BL2

unset LDFLAGS;

unset CFLAGS;

then lauch the build.

Regards,

Olivier

NRixh.1
Associate

Hi OlivierK,

Sorry for the disappointment. I don't know why I saw that I had to only unset LDFLAGS.

Regards,

Nicolas