STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Custom machine using meta-st-stmp32-addons on "Dunfell" doesnt create tf-a/custom-machine-trusted.dtb.

Hi experts and community!(Still on DISTRO_VERSION      = "3.1.11-snapshot-20221108")Following the instructions https://wiki.stmicroelectronics.cn/stm32mpu/wiki/How_to_create_your_own_machineI tried to create a custom machine.mx└── stm32mp1-custom ...

GLaure by Senior
  • 2532 Views
  • 1 replies
  • 1 kudos

Debugging of Cortex M4 in Stm32MP157

Hello   We are using STM32MP157A-dk1 evaluation board. To this we are writing bare metal code in SEGGER Embedded Studio.   We have written code for all three cores (A7_0,A7_1,M4). Individually we are able to debug(with limitations), For final testing...

USB port 2 cannot be recognized!

We built a customised board based on the stm32mp175c-dk2, with some changes, one of which was the addition of two USB type-c connectors.When I try to use the USB in DFU mode, everything works fine, as long as the boot switch is turned off. When I tur...

0693W00000VOppRQAT.png 0693W00000VOpqAQAT.png