cancel
Showing results for 
Search instead for 
Did you mean: 

Needs support the Windows 10 IoT

yanming2013 mo
Associate II

Hi all,

Windows 10 IoT Core already supports run on the single ARM Cortex-A7 MPU! Is there a BSP of the STM32 MPU that can be used for the Windows 10 IoT?

Refer here:

https://docs.microsoft.com/en-us/windows/iot-core/learn-about-hardware/socsandcustomboards

Best Regards

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @yanming2013 mo​ 

In case in may fit your need we are supporting Microsoft AZURE IoT

Please refer to :

https://wiki.st.com/stm32mpu-ecosystem-v1/wiki/How_to_integrate_Azure_IoT_Edge_on_OpenSTLinux

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @Community member​ ,

Thanks for your reply.

The Azure IoT is totally not the same as the windows 10 IoT.

The Windows 10 IoT is a kind of OS that will instead of the Windows CE. The Azure IoT is a kind of the component and needs run on some OS like Windows 10 IoT or Linux.

As I knew that, the windows 10 IoT already supports the single-core of ARM Cortex-A7 and the STM32MP1 already can be supported by the Windows 10 IoT, but the BSP of the STM32MP1 should be supported by your team. 

Please refer here to get more information about the windows 10 IoT and BSP:

https://docs.microsoft.com/en-us/windows/iot-core/windows-iot-core

https://docs.microsoft.com/en-us/windows-hardware/manufacture/iot/create-a-new-bsp