cancel
Showing results for 
Search instead for 
Did you mean: 

License file (EULA) for new machine in custom layer not found

KChoj.2312
Associate II

Hi, I try to add a new layer and a new machine to the STM32MP1 Distribution Image. i followed the following tutorials tutorials:

https://wiki.st.com/stm32mpu/wiki/How_to_create_a_new_open_embedded_layer

https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Distribution_Package

However, I am still getting the following error:

WARNING: st-image-core-1.0-r0 do_populate_lic: Could not copy license file /home/user/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-st-stm32mp-addons/conf/eula/stm32mp1-mymachine to /home/user/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/build-openstlinuxeglfs-stm32mp1-mymachine/tmp-glibc/work/stm32mp1_mymachine-openstlinux_eglfs-linux-gnueabi/st-image-core/1.0-r0/license-destdir/st-image-core/stm32mp1-mymachine: [Errno 2] No such file or directory: '/home/user/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-st-stm32mp-addons/conf/eula/stm32mp1-mymachine'
ERROR: st-image-core-1.0-r0 do_populate_lic: QA Issue: st-image-core: LIC_FILES_CHKSUM points to an invalid file: /home/user/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-st-stm32mp-addons/conf/eula/stm32mp1-mymachine [license-checksum]
ERROR: st-image-core-1.0-r0 do_populate_lic: Fatal QA errors found, failing task.
ERROR: st-image-core-1.0-r0 do_populate_lic: Function failed: populate_lic_qa_checksum
ERROR: Logfile of failure stored in: /home/user/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/build-openstlinuxeglfs-stm32mp1-mymachine/tmp-glibc/work/stm32mp1_mymachine-openstlinux_eglfs-linux-gnueabi/st-image-core/1.0-r0/temp/log.do_populate_lic.30716
ERROR: Task (/home/user/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-core.bb:do_populate_lic) failed with exit code '1'

So it looks that the bibtake still looks for the license file in the meta-st-stm32mp-addons, but not in my layer directory. Is there something I need to add to the configuration described in the tutorials from stm32mp1 wiki? I have already created the conf/eula directory in my layer with the link stm32mp1-mymachine -> ST_EULA_SLA.

Best regards,

Krzysztof

This discussion is locked. Please start a new topic to ask your question.
15 REPLIES 15

I created the layer once again according to the wiki posts with the same directory names. It is located in the meta-st/meta-my-demo-layer/ directory/ - the error is still the same.

ll ../layers/meta-st/meta-my-demo-layer/conf/eula/
total 64
drwxrwxr-x 2 krzysiek krzysiek  4096 gru  4 14:23 ./
drwxrwxr-x 4 krzysiek krzysiek  4096 gru  4 14:23 ../
-rw-rw-r-- 1 krzysiek krzysiek  5533 gru  4 14:23 en.SLA0048.txt
-rw-rw-r-- 1 krzysiek krzysiek  4178 gru  4 14:23 LICENCE.broadcom_bcm43xx
-rw-rw-r-- 1 krzysiek krzysiek  8997 gru  4 14:23 LICENCE.cypress
-rw-rw-r-- 1 krzysiek krzysiek 21707 gru  4 14:23 ST_EULA_SLA
lrwxrwxrwx 1 krzysiek krzysiek    11 gru  4 14:23 stm32mp1-demo -> ST_EULA_SLA
-rw-rw-r-- 1 krzysiek krzysiek  2757 gru  4 14:23 Vivante_GPU_drivers-End_User_Software_License_Terms.txt
cat ../layers/meta-st/meta-my-demo-layer/conf/layer.conf 
# We have a conf and classes directory, add to BBPATH
BBPATH .= ":${LAYERDIR}"
 
# We have recipes-* directories, add to BBFILES
BBFILES += "${LAYERDIR}/recipes-*/*/*.bb \
            ${LAYERDIR}/recipes-*/*/*.bbappend"
 
BBFILE_COLLECTIONS += "meta-my-demo-layer"
BBFILE_PATTERN_meta-my-demo-layer = "^${LAYERDIR}/"
BBFILE_PRIORITY_meta-my-demo-layer = "7"
 
EULA_FILE_ST_stm32mpmydemo = "${LAYERDIR}/conf/eula/${MACHINE}"
EULA_FILE_ST_MD5SUM_stm32mpmydemo = "8b505090fb679839cefbcc784afe8ce9"
 
#Inform bitbake for adding another location to search for licenses
LICENSE_PATH += "${LAYERDIR}/files/licenses"
 
# Set a variable to get the STM32MP MX BSP location
STM32MP_MY_DEMO_BASE = "${LAYERDIR}"
 
# This should only be incremented on significant changes that may
# cause compatibility issues with other layers
LAYERVERSION_meta-my-demo-layer = "1"
LAYERDEPENDS_meta-my-demo-layer = "stm-st-stm32mp-mx"
LAYERSERIES_COMPAT_meta-my-demo-layer = "thud"
bitbake-layers show-layers
NOTE: Starting bitbake server...
layer                 path                                      priority
==========================================================================
meta-my-demo-layer    /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-my-demo-layer  7
meta-st-stm32mp-addons  /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-st-stm32mp-addons  7
meta-python           /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-openembedded/meta-python  7
meta-oe               /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-openembedded/meta-oe  6
meta-oe               /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-openembedded/meta-oe  6
meta-gnome            /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-openembedded/meta-gnome  7
meta-xfce             /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-openembedded/meta-xfce  7
meta-initramfs        /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-openembedded/meta-initramfs  8
meta-multimedia       /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-openembedded/meta-multimedia  6
meta-networking       /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-openembedded/meta-networking  5
meta-webserver        /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-openembedded/meta-webserver  6
meta-filesystems      /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-openembedded/meta-filesystems  6
meta-perl             /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-openembedded/meta-perl  6
meta-python           /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-openembedded/meta-python  7
meta-st-stm32mp       /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-st-stm32mp  6
meta-qt5              /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-qt5  7
meta-st-openstlinux   /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-st-openstlinux  5
meta                  /home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/openembedded-core/meta  5
bitbake -e | grep ^EULA_FILE_ST
EULA_FILE_ST="/home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-st-stm32mp-addons/conf/eula/stm32mp1-demo"
EULA_FILE_ST_MD5SUM="8b505090fb679839cefbcc784afe8ce9"
EULA_FILE_ST_MD5SUM_stm32mpcommon="8b505090fb679839cefbcc784afe8ce9"
EULA_FILE_ST_MD5SUM_stm32mpcommonmx="8b505090fb679839cefbcc784afe8ce9"
EULA_FILE_ST_MD5SUM_stm32mpmydemo="8b505090fb679839cefbcc784afe8ce9"
EULA_FILE_ST_stm32mpcommon="/home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-st-stm32mp/conf/eula/stm32mp1-demo"
EULA_FILE_ST_stm32mpcommonmx="/home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-st-stm32mp-addons/conf/eula/stm32mp1-demo"
EULA_FILE_ST_stm32mpmydemo="/home/krzysiek/workspace/STM32MP1/Distribution-Package/openstlinux-4.19-thud-mp1-19-10-09/layers/meta-st/meta-my-demo-layer/conf/eula/stm32mp1-demo"

 Krzysztof

It looks like you didn't set MACHINEOVERRIDES .= ":stm32mpmydemo" in your new machine.

When properly set you should get :

$> bitbake -e | grep ^MACHINEOVERRIDES

MACHINEOVERRIDES="armv7ve:stm32mp1-demo:stcommon:stm32mpcommon:stm32mpmydemo"

$> bitbake -e | grep ^EULA_FILE_ST

EULA_FILE_ST="<my path>/layers/meta-st/meta-my-demo-layer/conf/eula/stm32mp1-demo"

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Pay attention to put MACHINEOVERRIDES .= ":stm32mpmydemo" at the end of your conf file.

It might be the last one in the MACHINEOVERRIDES list.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Yeah... I have just moved it below the includes list and it looks that the error disappeared. I will verify it once again on a clean build and then on my own layer. Thanks for the help.

Krzysztof

Hi Olivier,

This was the real problem since the beginning. Thank you for help. It solved this issue in all layers I created.

Krzysztof

Thanks for feedback.

Sorry not to pointed out this earlier. :\

We are working to enhanced the wiki in order nobody else fall into the trap.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.