cancel
Showing results for 
Search instead for 
Did you mean: 

isolcpus kernel parameter is ignored - make use of one STM32MP257 core only?

HMüll.4
Senior

Hi,

I'm trying to run the whole ST-Linux-stuff on one core only to have the other one available for a time-consuming application. However, it seems the kernel-parameter isolcpus is not used, dmesg gives an output

[    0.000000] Kernel command line: root=PARTUUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582 rootwait rw   earlycon console=ttySTM0,115200 isolcpus=0
[    0.000000] Unknown kernel command line parameters "isolcpus=0", will be passed to user space.
[    2.309368]     isolcpus=0

The message is correct, also with this parameter set, the processes are spread over all cores.

What could be the problem here? 

Thanks!

 

1 ACCEPTED SOLUTION

Accepted Solutions
Erwan SZYMANSKI
ST Employee

Hello @HMüll.4 ,
I find it strange that you have this warning on your second line. I have it too using the same command line parameter as you have. However, using 1 as parameter, the warning is not here anymore and it seems to have the expected result.
Can you please make a try with isolcpus=1 instead of 0 ?

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Erwan SZYMANSKI
ST Employee

Hello @HMüll.4 ,
I find it strange that you have this warning on your second line. I have it too using the same command line parameter as you have. However, using 1 as parameter, the warning is not here anymore and it seems to have the expected result.
Can you please make a try with isolcpus=1 instead of 0 ?

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.