cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to connect an IMX477 on the STM32MPU157F-dk2

JJérô.1
Associate II

Hello,

When I plugged the IMX477 on a USB port and I have the following msg:

[ 7307.355686] usb 2-1.3: new high-speed USB device number 5 using ehci-platform

[ 7307.519593] uvcvideo: Found UVC 1.00 device Arducam IMX477 HQ Camera (0c45:636d)

[ 7307.534627] input: Arducam IMX477 HQ Camera: Arduc as /devices/platform/soc/5800d000.usbh-ehci/usb2/2-1/2-1.3/2-1.5

[ 7307.550269] usb 2-1.3: 3:1: cannot get freq at ep 0x84

[ 7308.295030] usb 2-1.3: 3:1: cannot get freq at ep 0x84

[ 7308.349280] usb 2-1.3: 3:1: cannot get freq at ep 0x84

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Olivier GALLIEN
ST Employee

Hi @JACQUES Jérôme​ ,

I'm not expert but I understand that such device may require some specific driver/support which does not looks to be by default in OpenSTLinux.

Which version of ecosystem are you using ?

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
JJérô.1
Associate II

Hi Olivier,

Thanks for you interest !

I'm using the 2.1. I see there is the 4.0 version maybe ....

A question Olivier, do you work in Sophia Antipolis ?

If yes, is it possible to have a meeting ?

Best regards,

Jérôme

Hello,
another question, issu it possible to connect the amicam1 with the stm32MPU157f-dk2?
Thanks a lot,
Jérôme