cancel
Showing results for 
Search instead for 
Did you mean: 

Install Ubuntu 18.04 (LTS) on STM32MP157D-EV1 board with starter package installed

kKim.1
Associate II

I am using the STM32MP157D-EV1 board.

The starter package is currently installed in EMMC boot mode.

the version is "ST OpenSTLinux - Weston - (A Yocto Project Based Distro) 4.0.4-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23 \n \l" .

I need to install Ubuntu 18.04 on this board, but I don't know how. 

Do I have to delete the installed package now and install Ubuntu 18.04?

Ah, I downloaded the ubuntu-18.04.6-desktop-amd64.iso file. 

I can use Windows 10 and Oracle virtualbox.

I want to use Windows 10 if possible, but if it's impossible, I can also use Oracle virtualbox.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Olivier GALLIEN
ST Employee

Hi @kKim.1​ ,

"I need to install Ubuntu 18.04 on this board"

This is not possible!

It looks like you mixed you PC / Host machine setup requiring Ubuntu 20.04 LTS and the STM32MP157D-EV1 target board which can only support the provided OpenSTLinux distribution.

Can you clarify ?

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @kKim.1​ ,

"I need to install Ubuntu 18.04 on this board"

This is not possible!

It looks like you mixed you PC / Host machine setup requiring Ubuntu 20.04 LTS and the STM32MP157D-EV1 target board which can only support the provided OpenSTLinux distribution.

Can you clarify ?

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.