cancel
Showing results for 
Search instead for 
Did you mean: 

yocto in stm32mp1

Anto_Z
Associate II

Hi, I'm new to yocto project, I'm trying to set password for  custom image in yocto in stm32mp157d-dk1(scarthgap) ,by editing the bb layer in image, its successfully build and flashed into SD card , but I'm trying to enter the login id and password , it says login Incorrect  ,I tried in all ways , but still it shows login incorrect ,

Anto_Z_0-1728038511821.png

I attached the Picture of the bb layer of my image above , Please anyone could tell me  what I'm missing there..

 

Anto_Z_1-1728038560263.png

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Erwan SZYMANSKI
ST Employee

Hello @Anto_Z ,
Are you sure the password is not blank here ? 

In you conf/local.conf file in <Yocto build folder>, we have a default setting that is :

EXTRA_IMAGE_FEATURES ?= "debug-tweaks"

This feature is supposed to remove password for root user. Maybe you can try to remove this feature and make another try.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Erwan SZYMANSKI
ST Employee

Hello @Anto_Z ,
Are you sure the password is not blank here ? 

In you conf/local.conf file in <Yocto build folder>, we have a default setting that is :

EXTRA_IMAGE_FEATURES ?= "debug-tweaks"

This feature is supposed to remove password for root user. Maybe you can try to remove this feature and make another try.

Kind regards,
Erwan.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PatrickF
ST Employee

Hi @Anto_Z 

please have a look to this post https://community.st.com/t5/stm32-mpus-embedded-software-and/the-root-password-how-to-set-during-compilation-the-openstlinux/m-p/618515

 

Note: the password is not stored in plaintext, you should generate the correct hash string using e.g.:

openssl passwd -5 xxxx  

Then as stated in the linked post, manually escape all $ with \ before copying in the usermod line

 

This link (in french) could help too: https://www.blaess.fr/christophe/yocto-lab/sequence-II-1/index.html#utilisateurs-et-mots-de-passe

 

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

Hi, Thanks for the help, i commented that line, and tried , then , I can't able to login as root , bcoz , commenting that line also remove the  root login, then i added the below line

EXTRA_IMAGE_FEATURES += "allow-root-login"

 and , i used encrypted password assignment instead of direct assignment ,  then, its worked fine

Hi , Thanks for the Help, I tried in the way mentioned in that post , now its working, Thank you