2022-11-09 9:40 AM
Hello everyone,
I need a way to synchronize A7 and M4 cores (find the same timestamp) within 1 ~ 2 usec. Is there any shared timer or resources except for memory and virtual serial com between these two cores? I have a PPS signal and I want A7 to be aware of its arrival, but it has a 10 usec latency from the moment the PPS signal arrives! I do appreciate it if you let me know about viable methods I can take to mitigate this issue.
Best,
Saeed
2022-11-23 8:37 AM
Hi @Community member
I don't have an out of the box solution, but maybe look at something around connecting your external PPS signal to two timers trigger input (to reset the counters simultaneously), one timer assigned to Linux, and one timer assigned to M4, both counting on a clock from same root (e.g. HSE).
Then by reading the relevant timers count when you need them on either A7 or M4 side, you will have an absolute time indication Vs the real signal occurrence.
For timestamping, you could also check reading STGENR which is available for both A7 and M4 (but STGEN cannot be synchronized to an external pin).
This post could also be of interest: https://community.st.com/s/question/0D53W00000oXAqhSAG
Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.