2025-08-28 3:03 AM
Hello,
I'm following the Getting started wiki for Developing on Arm® Cortex®-M33. I already installed the IDE and the MP2 Packages. Now I'm in the section "Modify, rebuild and reload the firmware" but I'm stuck in Step 2. Software Prerequisites. Because I don't know how to install the build environment as explained in the wiki. It seems like it is for linux development, but I am using Windows, so I don't have the "sudo" and "export" options.
Can someone help me to execute these lines in windows? or is there another alternative?
1-Install dependencies:
sudo apt-get install -y git curl wget build-essential libssl-dev python3 \
python3-pip cmake make libncurses52-Add CMake path into environment:
export PATH=<CMake path>/bin:$PATH
Thanks in advance,
David
2025-08-28 11:20 PM - edited 2025-08-29 4:22 AM
You can't follow that guide in a Windows environment without using a virtual machine (through WSL or VirtualBox). This is due you need to use the Developer package which is only supported in a Linux environment.
Therefore, you are right, the commands that you highlight are for a Linux environment, in which you don't need to modify the path. What I recommend you is use WSL2, despite its usage for development is experimental. The best option is using VirtualBox o VMware.
You could check this in the PC requisites entry in the wiki and in the Developer packages entry in the wiki.