cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP257F: start some M33 code out of a running Linux?

HMüll.4
Senior

Hi,

when the STM32MP257F cores are running a regular Linux: how can I start some code on the M33 core? Is there a device/interface available within Linux that allows to send some code to this core and execute it? Or do they share some memory? So how is it working practically?

Thanks :)

1 ACCEPTED SOLUTION

Accepted Solutions
Christophe Guibout
ST Employee

Hello @HMüll.4,

 

I would recommand to have a look into Linux remoteproc wiki page : I guess it will help.

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Christophe Guibout
ST Employee

Hello @HMüll.4,

 

I would recommand to have a look into Linux remoteproc wiki page : I guess it will help.

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.