stm32mp157c implementation initramfs
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-07-25 4:23 AM
Hi,
I usestm32mp157c and the filesystem runs emmc default. But I want it to change it and run at ramfs. I added
CONFIG_BLK_DEV_INITRD=y
CONFIG_RD_GZIP=y
CONFIG_RD_BZIP2=y
CONFIG_RD_LZMA=y
CONFIG_RD_XZ=y
CONFIG_RD_LZO=y
CONFIG_RD_LZ4=y
in kernel config file. Also,
DISTRO_FEATURES_append = " ram"
IMAGE_FSTYPES_append = " cpio.xz"
in local.conf. After above additon operation, i have
uImage-initramfs.bin
But I don't know how to set the settings in U-boot. Like where should the starting address be? Can you help me with this?
Regards.
Ali MesutInce
Solved! Go to Solution.
- Labels:
-
STM32MP15 Lines
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-07-25 5:21 AM
Hello @aliMesut​ ,
Did you already read this page ? https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#Flashlayout-tsv_file_to_load_and_start_kernel
It explains how to build linux with the initramfs inside or how to load it separately, but in this case you must indicates, in the linux bootargs, where the file is located.
Long time, I did that, but If I remember well, you have to specify the address with "initrd=".
This is a standard linux use case not related to OSTL, so you will find a lot of information on internet.
In a first case, I recommend you to try the solution of a Linux with embedded initramfs.
Best Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-07-25 5:21 AM
Hello @aliMesut​ ,
Did you already read this page ? https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#Flashlayout-tsv_file_to_load_and_start_kernel
It explains how to build linux with the initramfs inside or how to load it separately, but in this case you must indicates, in the linux bootargs, where the file is located.
Long time, I did that, but If I remember well, you have to specify the address with "initrd=".
This is a standard linux use case not related to OSTL, so you will find a lot of information on internet.
In a first case, I recommend you to try the solution of a Linux with embedded initramfs.
Best Regards,
Kevin
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'