cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157C DSI for a 4 lane LCD (1280*800) PIXELS

军胡.1
Associate

Hi:

I have a MIPI LCD ,the driver IC is S6D7AA0X04,the LCD brief shows that the data lane is 4,and the pixels is (1280x800) less than 1366*768,if LCD data lane is configurable,Can I drive it with the STM32MP157C?

thanks�?​

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
PatrickF
ST Employee

Hello,

It should work, with checking on your LCD that it should be set to use 2 data lanes and could support a bandwidth of 1Gbit/s per lane (required to support 1280x800 24bits 60fps).

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
debugging
Lead

Hello Patrick,

I have the same question for an MIPI LCD, 4 lanes with the MP1

it seems the LCD cannot be configured to 2 lanes with any pins

LCD chipset = HX8282-A/C / HX8696-A01

Resolution of 1024x600 16.7M and support colors

Tlpxm and Tlpxd are 50nsec Min and 75nsec max.

TTA-SUREs = 2xTlpxd

TTA-GETD = 5xTlpxd

TTA-GOD=4xTlpxd

How to check from the chipset or LCD datasheet it can support the timing ?