cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157C Bring up

WHe.1
Associate II

Hello

My borad can bring up from SD card. But can not boot from eMMC. When boot from eMMC. I can't get any message from the console. How can I find the trouble?

Thanks

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @WHe.1​ ,

Can you share exact reference of STM32MP15 sample and eMMC please ?

I understand you succeed to flash the eMMC with CubeProg right ?

Please share the log from SD Card boot .. it might provide us some insight about your platfom configuration setup.

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PatrickF
ST Employee

Hi @WHe.1​ 

In case of low level boot failure, please share Bootrom log. Please have a look to https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_code_overview#Debug_and_Error_messages

and

https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_trace_analyzer

If you don't use default eMMC pins, please share OTP3 and OTP5-7 values you setup.

Note that some eMMC won't boot with silicon Rev.B. See ES0438 for details.

Regards.

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here