2023-02-10 9:43 PM
I am trying to use the USB OTG in host mode, but it kept giving me the famous HANG! Soft Reset timeout GRSTCTL_CSFTRST error.
According to the datasheet, when we set the register, it should reset the core but also clear itself but the following condition checks if it is 0 or not.
if ((hsotg->hw_params.snpsid & DWC2_CORE_REV_MASK) <
(DWC2_CORE_REV_4_20a & DWC2_CORE_REV_MASK)) {
if (dwc2_hsotg_wait_bit_clear(hsotg, GRSTCTL,
GRSTCTL_CSFTRST, 10000)) {
dev_warn(hsotg->dev, "%s: HANG! Soft Reset timeout GRSTCTL_CSFTRST\n",
__func__);
return -EBUSY;
}Here is some debugging that I have done
GRSTCTL VALUE before reset: 0x80000400
GRSTCTL VALUE after reset: 0x80000401
GRSTCTL inside if condition: 0x80000001
Here you can see, it has even cleared the 10th bit itself but did not clear the bit 0.
Following is my device tree, I still consider myself a beginner, so I need help.
&usbotg_hs{
u-boot,dm-pre-reloc;
pinctrl-names = "default", "sleep";
pinctrl-0 = <&usbotg_hs_pins_a &usbotg_fs_dp_dm_pins_a>;
status = "okay";
/* USER CODE BEGIN usbotg_hs */
compatible = "st,stm32mp15-fsotg", "snps,dwc2"; /* Use full-speed integrated PHY */
vbus-supply = <&vbus_otg>; /* voltage regulator to supply Vbus */
reg = <0x49000000 0x10000>;
clocks = <&rcc USBO_K>;
clock-names = "otg";
resets = <&rcc USBO_R>;
reset-names = "dwc2";
interrupts = <GIC_SPI 98 IRQ_TYPE_LEVEL_HIGH>;
dr_mode = "otg";
//dr_mode = "peripheral";
g-rx-fifo-size = <256>;
g-np-tx-fifo-size = <32>;
g-tx-fifo-size = <128 128 64 64 64 64 32 32>;
maximum-speed = "full-speed";
phy_type = "serial";
/* USER CODE END usbotg_hs */
};If I am not setting the clock correctly, let's assume I should not get any value when I read any register, while I do get the value when I try to read any register.