2020-09-29 4:35 AM
I am currently working on a design based around the STM32MP157C (mounted in the Seeed SoM - STM32MP157C).
I am trying to connect to the M4 Core on the target but I cannot halt it. When I attempt to do it, the debugger can halt the A7 CPU0 but fails at stopping the A7 CPU1 (Error: timeout waiting for DSCR bit change).
The M4 is completely inaccessible.
When I try to access the cores from the OpenOCD telnet interface, I can list the targets and get the following output after issuing a reset halt command.
> reset halt
stlink_dap_op_connect(connect)
SWD DPIDR 0x6ba02477
Deferring arp_examine of STM32MP157CACx.cm4
Use arp_examine command to examine it manually!
Target not examined, will not halt after reset!
stlink_dap_op_connect(connect)
stlink_dap_op_connect(reconnect)
SWD DPIDR 0x6ba02477
SWD DPIDR 0x6ba02477
STM32MP157CACx.cpu0: ran after reset and before halt ...
STM32MP157CACx.cpu1: ran after reset and before halt ...
STM32MP157CACx.cm4: hardware has 6 breakpoints, 4 watchpoints
STM32MP157CACx.cpu0 rev 5, partnum c07, arch f, variant 0, implementor 41
target halted in Thumb state due to debug-request, current mode: Supervisor
cpsr: 0x800001f3 pc: 0x00010bbc
MMU: enabled, D-Cache: disabled, I-Cache: enabled
timed out while waiting for target halted
TARGET: STM32MP157CACx.cpu1 - Not halted
> targets
TargetName Type Endian TapName State
-- ------------------ ---------- ------ ------------------ ------------
0 STM32MP157CACx.ap1 mem_ap little STM32MP157CACx.tap halted
1 STM32MP157CACx.ap2 mem_ap little STM32MP157CACx.tap halted
2 STM32MP157CACx.axi mem_ap little STM32MP157CACx.tap halted
3 STM32MP157CACx.cpu0 cortex_a little STM32MP157CACx.tap halted
4 STM32MP157CACx.cpu1 cortex_a little STM32MP157CACx.tap running
5* STM32MP157CACx.cm4 cortex_m little STM32MP157CACx.tap resetBefore the command was issued, all targets but the cm4 were in the running state (the cm4 is always stuck in the reset state).
How can I access the core and load a program into it ?
Tool versions and configuration:
Solved! Go to Solution.
2020-09-30 12:01 AM
Hi @bfh_dls
Yes I confirm. You need to boot in engineering mode.
Olivier
2020-09-29 4:57 AM
Hi @bfh_dls ,
First please check it can not be due to well know issue described in this post :
Olivier
2020-09-29 5:18 AM
I don't think so, I want to access only the M4 core and have not even configured anything to boot on the A7 cores.
I have been reading up on the boot modes, if I understand correctly, the only way to access the M4 with nothing running on the A7 cores is through engineering mode ? (we are currently not booting in engineering mode).
2020-09-30 12:01 AM
Hi @bfh_dls
Yes I confirm. You need to boot in engineering mode.
Olivier