2024-03-12 11:36 PM
Hi,
The MP157F-DK2 comes with an SD card attached. Weston (ver 5.0.0) with DRM works well.
But if I want to run Weston(ver 10.0.1) on Buildroot, it will fail.
Do I need to build more packages for Weston?
I am using the version of Buildroot.
a. buildroot: remotes/origin/st/2023.02.6
b. buildroot-external-st: remotes/origin/st/2023.02.2
This is the failure log, and the attachment is the success log of the SD card that comes with the MP157F-DK2.
# export XDG_RUNTIME_DIR=/run/user/root
# mkdir --parents $XDG_RUNTIME_DIR
# chmod 0700 $XDG_RUNTIME_DIR
# weston --tty=1
[00:01:34.112] weston 10.0.1
https://wayland.freedesktop.org
Bug reports to: https://gitlab.freedesktop.org/wayland/weston/issues/
Build: 2021.05-10575-gae4a6e0c24
[00:01:34.113] Command line: weston --tty=1
[00:01:34.113] OS: Linux, 6.1.28, #1 SMP PREEMPT Tue Feb 20 15:20:37 CST 2024, armv7l
[00:01:34.113] Flight recorder: enabled
[00:01:34.113] Starting with no config file.
[00:01:34.114] Output repaint window is 7 ms maximum.
[00:01:34.114] Loading module '/usr/lib/libweston-10/drm-backend.so'
[00:01:34.118] initializing drm backend
[00:01:34.118] Trying weston_launch launcher...
[00:01:34.118] could not get launcher fd from env
[00:01:34.118] Trying direct launcher...
[00:01:34.123] using /dev/dri/card0
[00:01:34.123] DRM: supports atomic modesetting
[00:01:34.123] DRM: supports GBM modifiers
[00:01:34.123] DRM: supports picture aspect ratio
[00:01:34.123] Compiled without GBM/EGL support
[00:01:34.123] failed to initialize egl
[00:01:34.123] fatal: failed to create compositor backend
Would you give an advice?
Thanks for reading.
Solved! Go to Solution.
2024-04-09 2:00 PM
Hello @wG.1 ,
For question specific to buildroot, it is recommended to contact our partner that support buildroot on our STM32MP1 platforms:
Bootlin has developed specific support, demonstration configurations and documentation to help ST customers use Buildroot on STM32MP1 platforms.
See https://www.st.com/content/st_com/en/partner/partner-program/partnerpage/Bootlin.html
To address Bootlin technical support: buildroot-st-support@bootlin.com
Hope it helps,
Best Regards,
Kevin
2024-04-09 2:00 PM
Hello @wG.1 ,
For question specific to buildroot, it is recommended to contact our partner that support buildroot on our STM32MP1 platforms:
Bootlin has developed specific support, demonstration configurations and documentation to help ST customers use Buildroot on STM32MP1 platforms.
See https://www.st.com/content/st_com/en/partner/partner-program/partnerpage/Bootlin.html
To address Bootlin technical support: buildroot-st-support@bootlin.com
Hope it helps,
Best Regards,
Kevin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.