2021-08-03 3:27 AM
Hello Team,
We are using a product build around STM32MP157C. We have a requirement for programming the OTP with MAC Id. Here is my understanding on the same:
We boot up our platform in basic mode. However, there was a mention that by default, OTP can be updated only in the secure mode. So, want to check if there is any setting which allows to update the MAC address specific OTP in basic mode?
Also, want to understand if there is any automated tool which would efficiently allows the MAC address to updated during the Mass Production?
2021-08-03 9:54 AM
Hello PTewa.1 (Community Member)
For 1 2 and 3. I can confirm,
OTP are programmed via the BSEC h/w peripheral (Boot, SEcurity and otp Control) which is a secured peripheral and configured at boot time. Basic U-boot does not have the security features to access the BSEC.
https://wiki.st.com/stm32mpu/wiki/BSEC_internal_peripheral
https://wiki.st.com/stm32mpu/wiki/BSEC_device_tree_configuration
STM32Cubeprogrammer can be used to program the OTP, although this is not a mass production programmer.
2021-08-03 5:29 PM
Hi Oliver,
Thanks for the quick reply.
Wanted to understand few things:
Regards,
Pradeep
Since STM32CubeProgrammer can be used to program the OTP
2021-08-04 8:52 AM
Hi PTewa.1 (Community Member)
Basic boot is not intended for production and does not embed secure services. It can only access the lower OTP from BSEC as non secure accesses.
https://wiki.st.com/stm32mpu/wiki/NVMEM_overview
As MAC address is part of the upper OTPs, it could accessed if TF-A as FSBL and U-Boot as SSBL are used.
STM32CubeProgrammer relies on the embedded secured Rom Code, TF-A and U-Boot to be able to program the OTPs. OEMs design their own tool based on this for production, or use it as is but at their own risks.
Regards,
Olivier
2021-08-04 10:07 AM
Hi Olivier,
Thanks for clarifying.
One follow up question - I understand u-boot can access the MAC address with fuse command in secure mode. So, provided the system is booted in secure mode, is it possible to program the MAC address from the user space using the sysfs interface for nvmem? This would allow the tool to be operated in user space with system booted up.
Regards,
Pradeep
2021-08-05 5:19 AM
Hi PTewa.1 (Community Member)
As mentioned in https://wiki.st.com/stm32mpu/wiki/NVMEM_overview
Only if a trusted boot chain is used, it is possible to access the upper OTPs via sysfs if already enabled in the BSEC device tree.
There is an exception management explained in order to allow some upper OTPs to be accessed by the non-secure world.
using the "st,non-secure-otp" definition
https://wiki.st.com/stm32mpu/wiki/BSEC_device_tree_configuration
Regards,
Olivier
2021-08-24 7:25 AM
Hi Olivier,
Thanks for the prompt response. I added the device tree node as suggested in https://wiki.st.com/stm32mpu/wiki/BSEC_device_tree_configuration as below:
&bsec {
mac_addr: mac_addr@e4 {
reg = <0xe4 0x8>;
st,non-secure-otp;
};
However still the OTP for MAC-ID is not accessible using the sysfs. Am I missing something? As per my understanding, adding the node in the DTB should allow an access to specific OTP words in non-secure mode.
The reason we don't want to switch to secure mode is that we have already designed & implemented the complete application using the non-secure mode and product is already in market. So, we are not sure of the implications which secure mode will bring in. And also, just for OTP update, switching to secure mode is somehow not working out for us. That's the reason we are looking for an alternative. And so far, what I understood from our conversations and the reference manual is that there is a way out to update the OTP in non-secure world. Please confirm if my understanding is correct.
Looking forward.
Regards,
Pradeep
2021-09-03 5:57 AM
Hello Pradeep,
Sorry for the late answer, the exception management explained in order to allow some upper OTPs to be accessed by the non-secure world (using the st,non-secure-otp in DT) requires anyway to go through secure world services for very specific needs, therefore it needs the Trusted boot chain.
The only way to update the OTP via the Basic boot chain is through the fuse command in U-boot, with a restriction of the LOCK that is not available.
How to update OTP with U-Boot - stm32mpu
Best Regards
Olivier