2023-01-05 7:21 PM
Hi all ~
I'm going to use proftpd to support FTP server.
first, I installed proftpd package from OpenSTLinux repository.
apt-get install proftpd And I tried to run proftpd with my configuration file.
but I got some error like below.
proftpd[5128]: fatal: unknown configuration directive 'AuthUserFile' As far as I know, proftpd has several modules related each features.
And the module I need is mod_auth_file.
so I checked proftpd's module list like below.
But there is no mod_auth_file module I want.
root@stm32mp1-prox-mx670:/home/hantas# proftpd -vv
ProFTPD Version: 1.3.7c (maint)
Scoreboard Version: 01040003
Built: Mon Aug 30 2021 00:22:56 UTC
Loaded modules:
mod_auth_pam/1.2
mod_facts/0.6
mod_delay/0.7
mod_site.c
mod_log/1.0
mod_ls.c
mod_auth.c
mod_auth_unix.c
mod_rlimit/1.0
mod_xfer.c
mod_core.cproftpd man page is described that mod_auth_file module is compiled by default.
But there is option to disable mod_auth_file module at compile time. (--disable-auth_file)
so I think, proftpd package offered by OpenSTLinux repository has above option.
In this case, is there any way to add proftpd module I want?
Or, Do I need to add proftpd recipe on my distribution package?
I'm not used to use yocto recipe yet.
Thank in advance for your answer.
Solved! Go to Solution.
2023-01-05 11:10 PM
Hi @hochul yoo
The recipe proftpd integrated into the OpenSTLinux distribution comes from the layer meta-openembedded (recipe meta-networking/recipes-daemons/proftpd/proftpd_1.3.7c.bb).
This recipe indeed disables by default the mod_auth_file module through the package configuration:
PACKAGECONFIG[auth] = "--enable-auth-file, --disable-auth-file"To enable it, you have to create a bbappend recipe proftpd_1.3.7c.bbappend in your own layer and to update the PACKAGECONFIG variable as followed:
PACKAGECONFIG:append = " auth"Best regards,
--JM
2023-01-05 11:10 PM
Hi @hochul yoo
The recipe proftpd integrated into the OpenSTLinux distribution comes from the layer meta-openembedded (recipe meta-networking/recipes-daemons/proftpd/proftpd_1.3.7c.bb).
This recipe indeed disables by default the mod_auth_file module through the package configuration:
PACKAGECONFIG[auth] = "--enable-auth-file, --disable-auth-file"To enable it, you have to create a bbappend recipe proftpd_1.3.7c.bbappend in your own layer and to update the PACKAGECONFIG variable as followed:
PACKAGECONFIG:append = " auth"Best regards,
--JM