2022-04-12 8:06 AM
Hello ,
I am building one application using Open gl es code. but gettign this error.Not sure if it is error as the final applications is building fine but giving error while elaunching .
No package 'wayland-client-protocol' found
Finished building target: my application
on launching this application it gives :
========== init_wayland_system ==========
Error : No such file or directory
can't connect to wayland display
========== init_wayland_system ==========
WHats happening here?
Regards,
D
2022-04-14 7:46 AM
Hello @darla14 ,
Could you please give me a little bit more information concerning your issue ?
Regards.
Erwan.
2022-04-18 9:48 PM
Hello @Erwan SZYMANSKI ,
thanks for the reply,
I cross-compiled the application using the mpu toolchain ( in sdk) for the starter package I flashed,. It has some code that runs on the gpu.
Difficult to share sc ...but i will check..
what issue do you see?
Br,
2022-04-22 3:10 AM
Hello @darla14 ,
sorry for late answer, are you still blocked ?
Ok no problem for the SC, can you share me your Makefile or your compilation options (CCFLAGS, LDFLAGS etc..) with masking sensitive information if there are ?
Rgs.
Erwan.
2022-04-22 5:41 AM
Moreover, do you have a weston service running when you try to execute your command ?
As far as I remember, using OpenGL ES with wayland-egl library needs it.
Regards.
Erwan.
2022-04-22 10:16 AM
Thanks @Erwan SZYMANSKI
Let me check on all these points and come back !
Br,
2022-06-09 5:11 AM
Hello @darla14 ,
Do you still need help on this issue?
Regards,
Kevin
2022-06-09 11:15 AM
Not now,thanks for the comment . @Kevin HUBER
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.