cancel
Showing results for 
Search instead for 
Did you mean: 

M33-TD: How to setup Yocto project

dmista
Associate II

How can I build the M33TD Yocto images from sources?

stm32mp2-m33td-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11

 

I managed to build the A35 flavor following this excellent summary:

Solved: stm32mp257f-EV1 yocto - STMicroelectronics Community

 

But now I would like to do the same for the M33TD boot mode. My board is a STM32MP257F-EV1

1 REPLY 1
Gregory PLANCHON
ST Employee

Hi @dmista ,

 

For this use case, you already have a machine name, stm32mp2-m33td. 

 

Regards,

Grégory 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.