cancel
Showing results for 
Search instead for 
Did you mean: 

ISO7816 interface of STM32MP135 to connect SAM (Secure Module Access) Card

OPetr.2
Associate II

Hi

I see the STM32MP135 has an ISO7816 interface. Have you developed a compatible Linux device driver for the ISO7816 interface? There exist a software framework to use the SAM (Secure Module Access) Card connected to this interface?

Thank you,

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Bernard PUEL
ST Employee

ISO7816 is supported in UART STM32 driver from V5.0.0 release but there is no framework in Linux to use it.