2019-08-12 8:42 AM
Hi. I have an STM32MPU157-DK2 Board in Engeneering mode.
i have power connected and the USB to the debug chip.
The Connection is successfully established.
I use a Terminal Programm to send and receive in hexadecimal numbers.
My Connectiondetails are 57600 Baud, 8N1
I send the first command 0x7F to establish a communication. it works.
all following commands are by hand so there is a little time between the commands.
I shorten the following communication a little bit,
me is my terminal & me,
bl is the bootloader
Me> 0x7F
BL> 0x79
Me> 0x00 0xFF
BL> 0x79 0x07 0x40 0x00 0x01 0x02 0x03 0x11 0x21 0x31 0x79
Me> 0x01 0xFE
BL> 0x79 0x10 0x00 0x00 0x79
Me> 0x02 0xFD
BL> 0x79 0x01 0x05 0x00 0x79
Me> 0x11 0xEE ( Read Memory)
BL> 0x79
Me> 0x10 0x00 0x00 0x00 0x10 (From 0x10000000,, SRAM1)
BL> 0x79
Me> 0x00 0xFF (1 Byte)
BL> 0x790xE0 0xE0 0xE0 0x00 0xE0 0xE0 0xE0 0x00 (...)
the output doesnt make much sense to me.
I tried several lengths (1 byte, 33 Bytes, 256 bytes)
and everytime there is several Kbytes of ****** data. all 00 or E0 or a few 0xFC and a few 0xF0. then the bootloader hangs. no communication is possibile anymore, i have to reset the board.
this does not make sense to me. I tried also several Areas,
0x00000000 ( Boot Rom), 0x2FFC0000 (Sysram)
all are not working....
what am i doing wrong?
Solved! Go to Solution.
2019-08-14 5:35 AM
Ok, i found out, just the beginnig of the SYSRAM gives those Problems.
if i read from the address 0x2FFC000 is breaks. But i read in the WIki that the first 9 Kbyte (0x2400) is used by the bootloader.
and if i read from 0x2FFC2400 it works!
great.
Next step: i will write my FSBL and start it.
2019-08-12 8:54 AM
My bad, i am in Serial boot, not egneneering boot.
additionally, i just noticed that there is an Command listed in the available commands that is not listed in the manual that i used (AN3155)
Command 0x03 0xFC gives me the answer 0x79 0x06 0x01 0x00 0x24 0xFC 0x2F 0x01 0x00 0x79
2019-08-14 5:35 AM
Ok, i found out, just the beginnig of the SYSRAM gives those Problems.
if i read from the address 0x2FFC000 is breaks. But i read in the WIki that the first 9 Kbyte (0x2400) is used by the bootloader.
and if i read from 0x2FFC2400 it works!
great.
Next step: i will write my FSBL and start it.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.