2022-02-12 4:25 PM
I am trying to build gui using GLADE designer for STM32 MP157 DK but i have problem in loading the generated GLADE XML in user space project.
Solved! Go to Solution.
2022-02-13 8:45 PM
Yes I understand. The problem is function call gtk_builder_add_from_file (GtkBuilder *builder, const gchar *filename GError **error ); Expects a filename that can be looked up in a file system.
Since you do not have a file system, you need to be using gtk_builder_add_from_string (GtkBuilder *builder const gchar *buffer gsize length GError **error ); which expects a pointer to character array with the array size of the character array. Follow these steps
Take the GLADE file you already have (I think you callled it "mygui.glade") and make is into a C array using the srec_cat utility, with the command line
srec_cat mygui.glade -Binary -o mygui.h -C-Array mygui_glade
This will produce a file called mygui.h containing a C array called mygui_glade There will also be a constant defining the size in the same H file
Now include the H file in your C code, and add the call gtk_builder_add_from_string (Builder, mygui_glade, mygui_glade_size, error); in all places where you called gtk_builder_add_from_file previously,
2022-02-12 8:05 PM
Convert it to a C array using srec_cat.exe, a free utility, available for Linux and windows. I use this to include TLC certificates in my project, using the command
srec_cat client-cert.pem -Binary -o client_cert.h -C-Array client_cert_pemThis converts the binary file "client-cert.pem" file into a C array called client_cert_pem in the file client_cert.h
Just substitute the name of your XML file, and include the H file in any of your C files.
2022-02-13 9:59 AM
@JMala.3
Hi,
Thanks for your reply. this is the code and its from example from youtube. the problem is in this part:
if(0 == gtk_builder_add_from_file (builder, "myui.glade", &err))
{
/* Print out the error. You can use GLib's message logging */
fprintf(stderr, "Error adding build from file. Error: %s\n", err->message);
/* Your error handling code goes here */
}
i created the file using glade designer and now i want to add it in stm32 cube ide user space project.
// My Application
//
// By (Your name)
// Libraries
#include <gtk-3.0/gtk/gtk.h>
#include <stdio.h>
// Variables
GtkWidget *window; // Window
GtkLabel *mylabel; // Label
GError *err = NULL; /* It is mandatory to initialize to NULL */
// Main function
int main(int argc, char *argv[])
{
GtkBuilder *builder; // GTK Builder variable
gtk_init(&argc, &argv); // Start GTK
builder = gtk_builder_new(); // Create GTK UI Builder
//gtk_builder_add_from_file(builder, "myui.glade", NULL); // Load our UI file
if(0 == gtk_builder_add_from_file (builder, "myui.glade", &err))
{
/* Print out the error. You can use GLib's message logging */
fprintf(stderr, "Error adding build from file. Error: %s\n", err->message);
/* Your error handling code goes here */
}
// Assign the Variables
window = GTK_WIDGET(gtk_builder_get_object(builder, "MyWindow")); // Load our window named MyWindow
mylabel = GTK_LABEL(gtk_builder_get_object(builder, "MyLabel")); // Load our label named MyLabel
// Essential for a GTK based program
gtk_builder_connect_signals(builder, NULL);
g_object_unref(builder);
gtk_widget_show_all(window); // Show our window
gtk_main(); // Run our program
return 0; // Necessary for a c main function
}
// Function to exit our app
void exit_app()
{
printf("Exit app \n"); // Not neccesary
gtk_main_quit(); // Command to quit a GTK program
}
// Function when our button is pressed
void button_clicked()
{
printf("Button clicked \n");
gtk_label_set_text(mylabel, "Hello World");
}
2022-02-13 8:45 PM
Yes I understand. The problem is function call gtk_builder_add_from_file (GtkBuilder *builder, const gchar *filename GError **error ); Expects a filename that can be looked up in a file system.
Since you do not have a file system, you need to be using gtk_builder_add_from_string (GtkBuilder *builder const gchar *buffer gsize length GError **error ); which expects a pointer to character array with the array size of the character array. Follow these steps
Take the GLADE file you already have (I think you callled it "mygui.glade") and make is into a C array using the srec_cat utility, with the command line
srec_cat mygui.glade -Binary -o mygui.h -C-Array mygui_glade
This will produce a file called mygui.h containing a C array called mygui_glade There will also be a constant defining the size in the same H file
Now include the H file in your C code, and add the call gtk_builder_add_from_string (Builder, mygui_glade, mygui_glade_size, error); in all places where you called gtk_builder_add_from_file previously,
2022-02-15 2:42 AM
@JMala.3
Thank you. your solution worked