cancel
Showing results for 
Search instead for 
Did you mean: 

How to flash the system without STM32CubeProgrammer

Ivy7
Associate II

Hello STMicroelectronics Community:

I would like to ask how to burn the system without using STM32CubeProgrammer. My chip is stm32mp135-AAE3.

 

Thanks,

Ivy7

3 REPLIES 3

Hi @Ivy7,

 

I could suggest that you have a look at the STM32 MPU wiki (https://wiki.st.com/stm32mpu/wiki/Main_Page).

 The following article might be interesting for you:

* https://wiki.st.com/stm32mpu/wiki/How_to_populate_the_SD_card_with_dd_command: it introduces a script running on Linux host PC to populate only the microSD card device (take care to retrieve the right volume name associated with the microSD card).

 

Hope this information helps.

 

Regards,

JC.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PatrickF
ST Employee

Hi @Ivy7 ,

 

you could also have a look to
https://www.st.com/en/partner-products-and-services/gang-flasher.html

or CubeProgrammer Command line for MPUs
See section 5 of UM2237: STM32CubeProgrammer software description

or CubeProgrammer API
See section 6 of UM2237: STM32CubeProgrammer software description

or if you want to build your own loader (heavy task I think)
AN5275: Introduction to USB DFU/USART protocols used in STM32MP1 and STM32MP2 MPU bootloaders

Btw, could you share the rationale of not using CubeProgrammer ? Speed ? Customization ? License ? else ?

 

Regards

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here

Hi,PatrickF:

 

Thank you for your answer, I will check out the above link you sent me.

The reason for  not using CubeProgrammer is that I want to batch burn the system,  but the factory doesn't  have the CubeProgrammer,  I want to provide them with another solution. 

 

Thanks,

Ivy7