2019-04-29 7:51 AM
2019-04-30 7:06 AM
Hi,
Please have a look to similar post in this Forum :
What is the process for initializing the OpenEmbedded build environment st-example-image-qt?
st-example-image-qt Qt examples extremely slow
Guess you will find hint you are looking for.
Olivier
2019-05-02 4:48 AM
Thank you for the links.
We were able to build the image - st-example-image-qt. However, we are facing issues while flashing it to the target device - STM32mpC157-DK2 .
Error Message: log
Memory Programming ...
Opening and parsing file: st-example-image-qt-openstlinux-eglfs-stm32mp1.ext4
File : st-example-image-qt-openstlinux-eglfs-stm32mp1.ext4
Size : 1086592 KBytes
Partition ID : 0x23
Download in Progress:
[=================================== ] 70%
Error: failed to download Segment[0]
Error: failed to download the File
Time elapsed during download operation: 00:11:25.623
Error: Download partition 0x23 failed
Error: TSV flashing service failed
Request for support!!
2019-05-06 8:12 AM
1/ Could you please check you did this (see above link) ?
conf/machine/include/st-machine-common-stm32mp.inc
# New value proposed for rootfs is 768MB
-ROOTFS_PARTITION_SIZE = "768432"
+ROOTFS_PARTITION_SIZE = "1400000"
2/ Could you please confirm you did flash this tsv ?
FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv