Hello,
i'd like to use u-boot command sspi to send commands to a spi device with a custom protocol (not a memory). However I see that the command tries to read an ID as it is talking to a flash nor : unrecognized JEDEC id bytes: 00, 00, 00.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-12-03 7:40 AM
Looking at the code, i see file sf_probe.c with .id = UCLASS_SPI_FLASH, that performs the id reading. How can i use stm32_spi.c with .id = UCLASS_SPI, driver instead? and send "raw" spi data?
Solved! Go to Solution.
- Labels:
-
STM32MP15 Lines
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-12-14 2:02 AM
Hello,
I added an alias for the spi and the command started working.
aliases {
serial0 = &uart4;
serial1 = &usart3;
spi1 = &spi1;
};
thank you
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-12-06 7:20 AM
Hi @Lmoio.1 ,
Can you share your Device Tree and particularly the spi node ?
Thx
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-12-06 7:45 AM
Hi @Community member,
My spi node definition in the device tree is the following:
&spi1 {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&spi1_pins_a>;
pinctrl-1 = <&spi1_sleep_pins_a>;
status = "okay";
cs-gpios = <&gpioe 12 0>;
spidev@0 {
compatible = "stm32_spi";
reg = <0>; /* CS #0 */
spi-max-frequency = <10000000>;
};
};
I inlcude arch/arm/dts/stm32mp151.dtsi file so
spi1: spi@44004000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "st,stm32h7-spi";
reg = <0x44004000 0x400>;
interrupts = <GIC_SPI 35 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&rcc SPI1_K>;
resets = <&rcc SPI1_R>;
dmas = <&dmamux1 37 0x400 0x01>,
<&dmamux1 38 0x400 0x01>;
dma-names = "rx", "tx";
power-domains = <&pd_core>;
status = "disabled";
};
I modified spi command to use the stm32 driver (but i'm not sure) instead of the spi_generic_drv driver:
ret = spi_get_bus_and_cs(bus, cs, freq, mode, "stm32_spi",
str, &dev, &slave);
I added some print in the driver files, and when doing sspi 0:0.0 8 a, i see that it performs sf_probe.c probing function (spi_flash_std_probe and spi_flash_probe_slave) and gives:
unrecognized JEDEC id bytes: 00, 00, 00.
I also tried disabling the spi flash driver, modifiying the defconfig with
CONFIG_ENV_IS_IN_SPI_FLASH=n
CONFIG_DM_SPI_FLASH=n
Now i see
spi_get_bus_and_cs: Binding new device 'generic_0:2', busnum=0, cs=2, driver=stm32_spi
But then it fails at line
priv->base = dev_remap_addr(dev);
in the stm32_spi.c file.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-12-09 8:50 AM
Hi @Community member
I worked some more on this issue and I noticed that inside spi-uclass.c file, the function ret = uclass_get_device_by_seq(UCLASS_SPI, busnum, &bus);
put in bus a udevice parent with name spi@58003000 that is the QSPI base address, is this a possible issue? How can I force to use spi@44004000 that is SPI1?
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-12-09 9:08 AM
Hi @Lmoio.1 ,
Sorry for late reply.
Looking at your DT this is the comment I can do :
The node spidev@0 supposed to refer to the device connected on SPI.
The compatible = "stm32_spi"; supposed to refer to this device driver ... provider or in-house code.
In this case it refer to anything and anyway not to the stm32_spi driver.
compatible = "st,stm32h7-spi"; is the only and correct binding to call stm32_spi driver.
To be use SPI1 as raw I even wonder if you need to define a device node.
Did you try to remove it ?
Hope it help,
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-12-10 1:28 AM
Hi @Community member
I tried command dm tree and noticed the following:
spi 0 [ ] stm32_spi | |-- spi@44004000
spi 1 [ + ] stm32_qspi | |-- spi@58003000
so I figured out that qspi was actually enabled. I disabled it in the device tree and now I don't see its entry anymore. However there is no "+" on the spi entry.
Why does the spy not get probed?
I removed the node as you mentioned,
&spi1 {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&spi1_pins_a>;
pinctrl-1 = <&spi1_sleep_pins_a>;
status = "okay";
cs-gpios = <&gpioe 12 0>;
};
now when i try sspi, i get
Invalid bus 0 (err=-19)
Are you able to use it somehow? Do you have a better idea if I need to send data to another stm32 mcu via spi during boot?
Thanks
Lidia
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-12-14 2:02 AM
Hello,
I added an alias for the spi and the command started working.
aliases {
serial0 = &uart4;
serial1 = &usart3;
spi1 = &spi1;
};
thank you
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-12-14 2:07 AM
Hi @Lmoio.1 ,
Well spotted !
For reference for others could you please confirm the working spi DT node for this usage ?
Thanks,
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-12-14 2:48 AM
Hi,
This is the device tree configuration i used
&spi1 {
u-boot,dm-spl;
pinctrl-names = "default", "sleep";
pinctrl-0 = <&spi1_pins_a>;
pinctrl-1 = <&spi1_sleep_pins_a>;
status = "okay";
cs-gpios = <&gpioz 3 0>;
};
and i also reverted all modifications i did in the spi.c uboot command.
To summarize:
- CONFIG_CMD_SPI=y in the defconfig
- qspi disabled in the device tree
- spi enabled and with alias in the device tree
- using the right bus "sspi 1:0.0 32 a"