2023-12-30 4:29 AM
Got this error in boot log.
[ 4.036653] stm32f7-i2c 5c009000.i2c: error -ENOENT: Failed to get controller clock
[ 4.054809] stm32f7-i2c: probe of 5c009000.i2c failed with error -25c009000 refers to i2c6. Below is the relevant section in the optee dts. I2C4 and I2C6 share a clock and I2C4 is working fine. I2C6 is mentioned in the eztpc node, so that ain't it either.
st,clksrc=<
CLK_CKPER_DISABLED
CLK_ETH_PLL4P
CLK_SDMMC12_PLL3R
CLK_STGEN_HSI
CLK_I2C46_HSI
CLK_SDMMC3_PLL3R
CLK_USBO_USBPHY
CLK_UART24_HSI
CLK_RNG1_CSI
CLK_MPU_PLL1P
CLK_AXI_PLL2P
CLK_MCU_PLL3P
CLK_RTC_LSI
CLK_MCO1_DISABLED
CLK_MCO2_DISABLED
>;The i2c6 section:
&i2c6{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&i2c6_pins_z_mx>;
pinctrl-1 = <&i2c6_sleep_pins_z_mx>;
status = "okay";
pcf85263: pcf85263@51 {
compatible = "nxp,pcf85263";
reg = <0x51>;
status = "okay";
};
};I2C4 was set up to 400kHz and I2C6 default, changing I2C4 to default didn't help.
Am I forgetting something? Full dts can be found here.
Solved! Go to Solution.
2024-01-02 5:26 AM
Hello @michiel.tjampens ,
I think you have to do the same as for i2c4, in your core/code/dts/kernel/stm32mp151a-tios-scmi.dtsi, as to know :
&i2c6 {
clocks = <&scmi_clk CK_SCMI_I2C6>;
resets = <&scmi_reset RST_SCMI_I2C6>;
};
Kind regards,
Erwan.
2024-01-02 5:26 AM
Hello @michiel.tjampens ,
I think you have to do the same as for i2c4, in your core/code/dts/kernel/stm32mp151a-tios-scmi.dtsi, as to know :
&i2c6 {
clocks = <&scmi_clk CK_SCMI_I2C6>;
resets = <&scmi_reset RST_SCMI_I2C6>;
};
Kind regards,
Erwan.
2024-01-02 9:22 AM - edited 2024-01-03 2:51 AM
Hello @Erwan SZYMANSKI
That did the trick.But any idea why i2c4 and i2c6 need to be mentioned in the scmi but i2c5 doesn't?
Also i2cdetect takes atleast a second per address... but does in the end find the rtc on the correct address.
Pull-ups are present, idle state is high etc.
2024-08-04 10:34 PM
I just fixed this same error after debugging this for a day by adding this line in the SCMI files. This is not mentioned in the WIKI , nor CubeMX generates the SCMI file, nor the WIKI mentions about adding the clocks to OPTEE and EZTPC.
I now have the same issue with i2cprobe -y 0 on I2C6, is is very slow and takes one second per address. There are no devices on the bus. . I used the same code for i2cprobe for an MCU and that does not show such behavior
Is this normal or indicate a problem ? AFAIK, I2Cprobe just pulls the lines high and low and see if something happens, like basic GPIO.