cancel
Showing results for 
Search instead for 
Did you mean: 

BLE MAC Address is the same for all the SMT32MP1 [43:43:A1:12:1F:AC]

FFont.1
Associate II

Hello,

I'm trying to set-up a BLE GATT service and I'm struggling with the fact of the MAC address being the same for all the STM32MP1 devices.

When I run the hcitool dev this is what I get:

root@stm32mp1:~# hcitool dev

Devices:

hci0 43:43:A1:12:1F:AC

Please help

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Probably because an allocation costs money.

For test purposes make sure each within your experiment is unique

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thank you for the reply.

However, I'm not understanding your answer. Are you saying that these MP1 processors don't have an allocated BLE MAC address?

I thought this was an issue with the bluez library as referred here: https://www.raspberrypi.org/forums/viewtopic.php?t=191534.

How can I have multiple devices running at the same time with this non-unique MAC address?